u-boot for custom board i.MX6SL with DDR3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

u-boot for custom board i.MX6SL with DDR3

跳至解决方案
3,120 次查看
pawelkrzyzanows
Contributor II

Hi,

I am trying to get any response from my custom board (close to SLEVK) although DDR3 instead of LPDDR2. All I want is to get U-boot working. To download u-boot to board I use, 'imx_usb'.

HARDWARE:

i.MX6SL and DDR3 Micron: 2x MT41K128M16JT-125. --> USB OTG Communication (lsusb --> Bus 001 Device 025: ID 15a2:0063 Freescale Semiconductor, Inc)

Steps I made:

- Calculate DDR3 Timings by using I.MX6DQSDL DDR3 Script Aid V0.10xlsx (attached)

- Prepare flash_header.s (attached) (and put it board->freescale->mx6sl_evk)

- build u-boot.bin

- imx_usb u-boot.bin  (and here problems begin)

 

After those step I expect to get u-boot > prompt in serial UART1. But on any UART available I don't get any response.

 

(I try with several modify flash_header.s, I can get two types of response. First if I set to use DDR3:

HAB security state: development mode (0x56787856) == work item filename u-boot.bin load_size 0 bytes load_addr 0x00000000 dcd 1 clear_dcd 0 plug 1 jump_mode 2 jump_addr 0x00000000 == end work item main dcd length 1e0 sub dcd length 1dc  loading binary file(u-boot.bin) to 87800000, skip=0, fsize=272b4 type=aa out err=-7, last_trans=0 cnt=0x3c00 max=0x400 transferSize=0x400 retry=0

 

and error retry 10 times and no communication. Or if use flash_header.s oryginal form sl_evk (LPDDR2) I can get "success" but nothing appears on UART:

HAB security state: development mode (0x56787856) == work item filename u-boot.bin load_size 0 bytes load_addr 0x00000000 dcd 1 clear_dcd 0 plug 1 jump_mode 2 jump_addr 0x00000000 == end work item main dcd length 248 sub dcd length 244  loading binary file(u-boot.bin) to 87800000, skip=0, fsize=27134 type=aa  <<<160052, 160052 bytes>>> succeeded (status 0x88888888) jumping to 0x87800400

 

I also check my board by using Freescale DDR Stress Tester 2.2 and attach logs. I can download configuration form board. I can even launch stress test/calibration and get some results. But no matter what I try to do no communication on UART...

 

Any hints/reasons why I can't get any response? Where to search?

Original Attachment has been moved to: ddr_calibration_20151117-15'1'37.log.zip

Original Attachment has been moved to: ddr_stresstest_20151118-15'4'25.log.zip

标签 (3)
标记 (2)
0 项奖励
回复
1 解答
2,548 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Pawel

please look at attached Porting Guide and

i.MX6SL DDR3 support for L3.0.35_2.1.0

also one can connect jtag and check uart iomux settings.

It is recommended to use tools from i.MX6SL EVK product page, as

FSL does not support 'imx_usb'.

i.MX 6SoloLite Evaluation Kit|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,549 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Pawel

please look at attached Porting Guide and

i.MX6SL DDR3 support for L3.0.35_2.1.0

also one can connect jtag and check uart iomux settings.

It is recommended to use tools from i.MX6SL EVK product page, as

FSL does not support 'imx_usb'.

i.MX 6SoloLite Evaluation Kit|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,548 次查看
pawelkrzyzanows
Contributor II

Thank You for the links.

I found the hint I was missing in my file :smileyhappy:

I use tool's for MX6SL_EVK (MFG) but they stuck and can't load any boot to board, and because I am compiling u-boot on Linux machine it is easier to use command line Linux tool.

Anyway I am staring to lunch kernel and hope will manage do this :smileyhappy:

0 项奖励
回复