i.MX 6UltraLite eMCP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6UltraLite eMCP

2,012 Views
ricardoferreira
Contributor II

Hi,
Did anybody design a 32bit LPDDR2 with i.MX 6UltraLite.

For example, is it possible to use the eMCP MT29PZZZ4D4BKESK18 from micron?

Thank you very much in advance.


Regards,
Ricardo F.

Labels (1)
2 Replies

1,851 Views
BiyongSUN
NXP Employee
NXP Employee

i.MX6UL DDR controller is 16 bit.

1,851 Views
ricardoferreira
Contributor II

Hi,
Thank you for your answer.

Based on the datasheet of this memory the component can handle both x16 and x32 width. So, probably it is only the matter of loosing the bandwidth.

Based on the datasheet of the IMX6UL it can support LPDDR2 as well. So do you think that we can have problems?

0 Kudos
Reply