u-boot changes for iMX8MM based custom DDR 1GB RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot changes for iMX8MM based custom DDR 1GB RAM

4,391 Views
siva_prabhakara
Contributor III

hi ,

we are making a custom board based on i.MX8M mini but the DDR is 1GB RAM.

I figured out that NXP provides a DDR tool here https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

and the code updates needed in u-boot as per Clock frequency and 1GB size change as mentioned in https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-8M-Mini-Register-Programming-Aid-DRA...

Any changes needed for TEE?

0 Kudos
Reply
4 Replies

3,580 Views
AmiraniTurmanidze
Contributor I

Hi.
I have problem with training:
Screenshot 2023-11-06 183013.png

This is schematic of our custom MPU module. It works perfect with 2GB RAM...but no luck with 1GB(I use MScale DDR tool with RPA configurator)
RAM part number: MT53D512M16D1DS-046 TW:D

Can someone advice where to look for changes? This particular RAM doesn't have a Bank B.

0 Kudos
Reply

4,374 Views
igorpadykov
NXP Employee
NXP Employee

Hi siva_prabhakara

 

additional change details were sent via mail.

 

Best regards
igor

3,589 Views
AmiraniTurmanidze
Contributor I
Can I have this details?
0 Kudos
Reply

4,145 Views
don_gunn
Contributor V

Could I please get these additional changes?

0 Kudos
Reply