the same sensor is no image output when use palntform Mx6q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

the same sensor is no image output when use palntform Mx6q

1,427 次查看
gillianyang
Contributor I

Hi all

   we use parall port to conect camera sensor(16bit), the clk,hsys and vsys are from camera sensor,when we use other plantform, the image perform well,but when use MX6q,there is no image output,the log is attached below,compared the same sensor with dfiffrent plantform,the orange waveform is correct by use i.Mx515,and the green waveform is not good by use Mx6q,the waveform is attached below,.hope your reply!

0 项奖励
回复
1 回复

1,354 次查看
igorpadykov
NXP Employee
NXP Employee

Hi gillian

both IPU modules for i.MX515 and i.MX6Q basically the same, so may be

useful to run and compare IPU/CSI settings with baremetal sdk examples,

zip can be found on below link

SMP Enable in IMX6 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复