the question about internal ADC reference voltage -- i.mx257

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the question about internal ADC reference voltage -- i.mx257

Jump to solution
1,908 Views
王剑翰
Contributor III

We want to use the internal ADC reference voltage but we did not find the related information about the accuracy range and temperature drift characteristics of the internal ADC reference voltage.

I only find "The internal reference is fixed at 2.5 V", but I am not sure the accuracy range.

Could you kindly help me for this question?

Labels (1)
0 Kudos
Reply
1 Solution
1,745 Views
igorpadykov
NXP Employee
NXP Employee

Hi 王

the internal reference voltage accuracy is 4%

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
1,746 Views
igorpadykov
NXP Employee
NXP Employee

Hi 王

the internal reference voltage accuracy is 4%

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,745 Views
王剑翰
Contributor III

Hi Igor,

Thank you for your kindly answer.

Is the voltage accuracy ±4%?What is the temperature drift characteristics?

Could you kindly show me the related document?

0 Kudos
Reply
1,745 Views
igorpadykov
NXP Employee
NXP Employee

Hi 王

temperature drift included in that value

~igor

1,745 Views
王剑翰
Contributor III

Hi Igor,

Thank you for your kindly answer.

I think these specific should be noted in some document, but I can not find it.

Could you kindly show me the related document?

0 Kudos
Reply
1,745 Views
igorpadykov
NXP Employee
NXP Employee

Hi 王

that value is is from internal documents.

It is not from public documents.

~igor