switch position after boot iMX8MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

switch position after boot iMX8MP

2,007 Views
dhirajtarole
Contributor III

Hi,

I am using iMX8M Plus - 8MPLUSLPD4-EVK.

Device is boot with prebuilt linux and switch position is SW4 --  0010 (eMMC).

After Boot when we off the board and power on the board, it will start boot again.

Do i need to put SW4 position at -1110  (infinite loop) after board is booted ,when EVK is on.


Thanks,

 

 

 

 

 
 

 

 

 

 

 

0 Kudos
Reply
3 Replies

1,986 Views
joanxie
NXP TechSupport
NXP TechSupport

no you don't need to, did  you use nxp evk board and demo images? which bsp version do you use

0 Kudos
Reply

1,979 Views
dhirajtarole
Contributor III

Hi @joanxie ,

thanks for Reply, got the answer.

I have another query:-

I am trying to test CAN in android 11.0.0_2.2.0 in imx8mp (8MPLUSLPD4-EVK) but i am unable to up the CAN through debug terminal. i have tried multiple way and searched documents  for CAN communication in Android 11.0.0.

pls let me know

is it supported in this android version ? if yes than how can i test CAN.

for your reference attaching the image.

dhirajtarole_0-1668155451845.png

 

Thanks in advance,

Dhiraj

0 Kudos
Reply

1,970 Views
joanxie
NXP TechSupport
NXP TechSupport

pls check if your bsp enable flexCAN or not, check the configuration CONFIG_CAN_FLEXCAN, if you need detailed information about this, pls submit a ticket for this

 

0 Kudos
Reply