start kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

start kernel

966件の閲覧回数
Brilliant
Contributor I

I currently have two base boards, one of them is working, we call it board A for the sake of description, and the other one is under debugging, we call it board B. Now I burned the kernel into IMX6U normally on board A, and it also boots normally.But when I put the IMX6U in the B board, it keeps printing the following message and can't enter the system, can you tell me what causes it?

[ 4.973429] ERROR: v4l2 capture: slave not found!
[ 4.978200] imx-uart 2020000.serial: Rx FIFO overrun
[ 17.564390] usb 1-1: new high-speed USB device number 4 using ci_hdrc
[ 17.570923] imx-uart 2020000.serial: Rx FIFO overrun
[ 28.034347] usb 1-1: device not accepting address 4, error -110
[ 28.040359] imx-uart 2020000.serial: Rx FIFO overrun
[ 28.164347] usb 1-1: new high-speed USB device number 5 using ci_hdrc
[ 28.170869] imx-uart 2020000.serial: Rx FIFO overrun

0 件の賞賛
返信
0 返答(返信)