signed Kernel image and signed dtb launch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

signed Kernel image and signed dtb launch

1,060 次查看
antonio_santagi
Contributor IV

Hello,

once u-boot determines with hab_auth_img() that signed kernel image is correct and signed dtb file is correct , which is the correct command to launch that kernel image ? is it needed to extract the start address from boot data table or is there already a command for this ?

And for the dtb ?

thank you 

标记 (2)
0 项奖励
回复
1 回复

983 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  You may look at bootcmd command of U-boot in its environment. 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 项奖励
回复