signed Kernel image and signed dtb launch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

signed Kernel image and signed dtb launch

1,022件の閲覧回数
antonio_santagi
Contributor IV

Hello,

once u-boot determines with hab_auth_img() that signed kernel image is correct and signed dtb file is correct , which is the correct command to launch that kernel image ? is it needed to extract the start address from boot data table or is there already a command for this ?

And for the dtb ?

thank you 

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

945件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  You may look at bootcmd command of U-boot in its environment. 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信