sgtl5000 latency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sgtl5000 latency

1,863件の閲覧回数
dtran11
Contributor I

Using an iMX6 and SGTL5000 for audio, I noticed a 400ms delay when snd_pcm_prepare() is called. Looking at the sgtl5000.c codec driver, there is a sleep of 400ms when the power management powers up and powers down. For some reason the call to power up is always called on snd_pcm_prepare() even when the audio codec power never went down. I added a state to keep track of it in the codec driver as a workaround to not delay unless necessary. While this workaround works, I don't think it's the best solution. Does someone know why the power up section of code is always called in the driver? Thanks

+diff --git a/sound/soc/codecs/sgtl5000.c b/sound/soc/codecs/sgtl5000.c
+index 6668845..3aaf384 100644
+--- a/sound/soc/codecs/sgtl5000.c
++++ b/sound/soc/codecs/sgtl5000.c
+@@ -152,6 +152,8 @@ static int mic_bias_event(struct snd_soc_dapm_widget *w,
+ static int power_vag_event(struct snd_soc_dapm_widget *w,
+  struct snd_kcontrol *kcontrol, int event)
+ {
++ static bool is_power_up = false;
++
+  struct snd_soc_codec *codec = snd_soc_dapm_to_codec(w->dapm);
+  const u32 mask = SGTL5000_DAC_POWERUP | SGTL5000_ADC_POWERUP;
+
+@@ -159,7 +161,12 @@ static int power_vag_event(struct snd_soc_dapm_widget *w,
+  case SND_SOC_DAPM_POST_PMU:
+   snd_soc_update_bits(codec, SGTL5000_CHIP_ANA_POWER,
+    SGTL5000_VAG_POWERUP, SGTL5000_VAG_POWERUP);
+-  msleep(400);
++
++  if (is_power_up == false)
++  {
++   msleep(400);
++   is_power_up = true;
++  }
+   break;
+
+  case SND_SOC_DAPM_PRE_PMD:
+@@ -173,6 +180,7 @@ static int power_vag_event(struct snd_soc_dapm_widget *w,
+    snd_soc_update_bits(codec, SGTL5000_CHIP_ANA_POWER,
+     SGTL5000_VAG_POWERUP, 0);
+    msleep(400);
++   is_power_up = false;
+   }
+   break;
+  default: 

0 件の賞賛
返信
1 返信

1,731件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dat

seems power up and down is performed in driver for reducing overall board power consumption.

May be useful to check how power is handled in baremetal i.MX6 SDK sgtl5000 tests

(zip is available on https://community.nxp.com/thread/432859  )

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信