sdma memory to meory error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sdma memory to meory error

1,429 Views
sharpjison
Contributor II

software : Linux-4.1.18

hardware: I.MX6q

The file imx-sdma.c is linux/driver/dma/imx-sdma.c.

Error line :  dma_m2m_desc = dma_m2m_chan->device->device_prep_dma_sg(dma_m2m_chan,sg2, 3, sg, 3, 0);

                   dma_m2m_desc = dma_m2m_chan->device->device_prep_dma_memcpy(dma_m2m_chan, dma_dst, dma_src, SDMA_BUF_SIZE,0);

                   The two dma_m2m2_desc is all null

                  

#include <linux/module.h>
#include <linux/slab.h>
#include <linux/sched.h>
#include <linux/mman.h>
#include <linux/init.h>
#include <linux/dma-mapping.h>
#include <linux/fs.h>
#include <linux/version.h>
#include <linux/delay.h>
#if (LINUX_VERSION_CODE >= KERNEL_VERSION(3,0,35))
#include <linux/platform_data/dma-imx.h>
#else
#include <mach/dma.h>
#endif

 

#include <linux/dmaengine.h>
#include <linux/device.h>

 

#include <linux/io.h>
#include <linux/delay.h>

 

static int gMajor; /* major number of device */
static struct class *dma_tm_class;
u32 *wbuf, *wbuf2, *wbuf3, *wbuf4;
u32 *rbuf, *rbuf2, *rbuf3, *rbuf4;

 

struct dma_chan *dma_m2m_chan;

 

struct completion dma_m2m_ok;

 

struct scatterlist sg[3], sg2[3];

 

#define SDMA_BUF_SIZE  1024

 

 

 

static bool dma_m2m_filter(struct dma_chan *chan, void *param)
{
    if (!imx_dma_is_general_purpose(chan))
        return false;
    chan->private = param;
    return true;
}

 

int sdma_open(struct inode * inode, struct file * filp)
{
    dma_cap_mask_t dma_m2m_mask;
    struct imx_dma_data m2m_dma_data = {0};

 

    init_completion(&dma_m2m_ok);

 

    dma_cap_zero(dma_m2m_mask);
    dma_cap_set(DMA_SLAVE, dma_m2m_mask);
    m2m_dma_data.peripheral_type = IMX_DMATYPE_MEMORY;
    m2m_dma_data.priority = DMA_PRIO_HIGH;

 

    dma_m2m_chan = dma_request_channel(dma_m2m_mask, dma_m2m_filter, &m2m_dma_data);
    if (!dma_m2m_chan) {
        printk("Error opening the SDMA memory to memory channel\n");
        return -EINVAL;
    }

 

    wbuf = kzalloc(SDMA_BUF_SIZE, GFP_DMA);
    if(!wbuf) {
        printk("error wbuf !!!!!!!!!!!\n");
        return -1;
    }

 

    wbuf2 = kzalloc(SDMA_BUF_SIZE/2, GFP_DMA);
    if(!wbuf2) {
        printk("error wbuf2 !!!!!!!!!!!\n");
        return -1;
    }

 

    wbuf3 = kzalloc(SDMA_BUF_SIZE, GFP_DMA);
    if(!wbuf3) {
        printk("error wbuf3 !!!!!!!!!!!\n");
        return -1;
    }

 

    wbuf4 = kzalloc(SDMA_BUF_SIZE, GFP_DMA);
    if(!wbuf4) {
        printk("error wbuf4 !!!!!!!!!!!\n");
        return -1;
    }

 

    rbuf = kzalloc(SDMA_BUF_SIZE, GFP_DMA);
    if(!rbuf) {
        printk("error rbuf !!!!!!!!!!!\n");
        return -1;
    }

 

    rbuf2 = kzalloc(SDMA_BUF_SIZE/2, GFP_DMA);
    if(!rbuf2) {
        printk("error rbuf2 !!!!!!!!!!!\n");
        return -1;
    }

 

    rbuf3 = kzalloc(SDMA_BUF_SIZE, GFP_DMA);
    if(!rbuf3) {
        printk("error rbuf3 !!!!!!!!!!!\n");
        return -1;
    }

 

    rbuf4 = kzalloc(SDMA_BUF_SIZE, GFP_DMA);
    if(!rbuf4) {
        printk("error rbuf4 !!!!!!!!!!!\n");
        return -1;
    }

 

    return 0;
}

 

int sdma_release(struct inode * inode, struct file * filp)
{
    dma_release_channel(dma_m2m_chan);
    dma_m2m_chan = NULL;
    kfree(wbuf);
    kfree(wbuf2);
    kfree(wbuf3);
    kfree(wbuf4);
    kfree(rbuf);
    kfree(rbuf2);
    kfree(rbuf3);
    kfree(rbuf4);
    return 0;
}

 

ssize_t sdma_read (struct file *filp, char __user * buf, size_t count,
                                loff_t * offset)
{
    int i;

 

    for (i=0; i<SDMA_BUF_SIZE/4; i++) {
        if (*(rbuf+i) != *(wbuf+i)) {
            printk("buffer 1 copy falled!\n");
            return 0;
        }
    }
    printk("buffer 1 copy passed!\n");

 

    for (i=0; i<SDMA_BUF_SIZE/2/4; i++) {
        if (*(rbuf2+i) != *(wbuf2+i)) {
            printk("buffer 2 copy falled!\n");
            return 0;
        }
    }
    printk("buffer 2 copy passed!\n");

 

    for (i=0; i<SDMA_BUF_SIZE/4; i++) {
        if (*(rbuf3+i) != *(wbuf3+i)) {
            printk("buffer 3 copy falled!\n");
            return 0;
        }
    }
    printk("buffer 3 copy passed!\n");

 

#if (LINUX_VERSION_CODE >= KERNEL_VERSION(3,0,35))
    for (i=0; i<SDMA_BUF_SIZE/4; i++) {
        if (*(rbuf4+i) != *(wbuf4+i)) {
            printk("buffer 4 copy falled!,r=%x,w=%x,%d\n", *(rbuf4+i), *(wbuf4+i), i);
            return 0;
        }
    }
    printk("buffer 4 copy passed!\n");
#endif
    return 0;
}

 

static void dma_m2m_callback(void *data)
{
    printk("in %s\n",__func__);
    complete(&dma_m2m_ok);
    return ;
}

 

ssize_t sdma_write(struct file * filp, const char __user * buf, size_t count,
                                loff_t * offset)
{
    u32 *index1, *index2, *index3, i, ret;
    struct dma_slave_config dma_m2m_config = {0};
    struct dma_async_tx_descriptor *dma_m2m_desc;
    u32 *index4 = wbuf4;
    dma_addr_t dma_src, dma_dst;

 

    index1 = wbuf;
    index2 = wbuf2;
    index3 = wbuf3;

 

    for (i=0; i<SDMA_BUF_SIZE/4; i++) {
        *(index1 + i) = 0x12121212;
    }

 

    for (i=0; i<SDMA_BUF_SIZE/2/4; i++) {
        *(index2 + i) = 0x34343434;
    }

 

    for (i=0; i<SDMA_BUF_SIZE/4; i++) {
        *(index3 + i) = 0x56565656;
    }

 

    for (i=0; i<SDMA_BUF_SIZE/4; i++) {
        *(index4 + i) = 0x56565656;
    }

 

#if 0
    for (i=0; i<SDMA_BUF_SIZE/4; i++) {
    printk("input data_%d : %x\n", i, *(wbuf+i));
    }

 

    for (i=0; i<SDMA_BUF_SIZE/2/4; i++) {
    printk("input data2_%d : %x\n", i, *(wbuf2+i));
    }

 

    for (i=0; i<SDMA_BUF_SIZE/4; i++) {
    printk("input data3_%d : %x\n", i, *(wbuf3+i));
    }
#endif
    dma_m2m_config.direction = DMA_MEM_TO_MEM;
    dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_2_BYTES;
    dmaengine_slave_config(dma_m2m_chan, &dma_m2m_config);

 

    sg_init_table(sg, 3);
    sg_set_buf(&sg[0], wbuf, SDMA_BUF_SIZE);
    sg_set_buf(&sg[1], wbuf2, SDMA_BUF_SIZE/2);
    sg_set_buf(&sg[2], wbuf3, SDMA_BUF_SIZE);
    ret = dma_map_sg(NULL, sg, 3, dma_m2m_config.direction);

 

#if (LINUX_VERSION_CODE <= KERNEL_VERSION(3,0,35))
    dma_m2m_desc = dma_m2m_chan->device->device_prep_slave_sg(dma_m2m_chan,sg, 3, dma_m2m_config.direction, 1);
#endif

 

    sg_init_table(sg2, 3);
    sg_set_buf(&sg2[0], rbuf, SDMA_BUF_SIZE);
    sg_set_buf(&sg2[1], rbuf2, SDMA_BUF_SIZE/2);
    sg_set_buf(&sg2[2], rbuf3, SDMA_BUF_SIZE);
    ret = dma_map_sg(NULL, sg2, 3, dma_m2m_config.direction);

 

#if (LINUX_VERSION_CODE <= KERNEL_VERSION(3,0,35))
    dma_m2m_desc = dma_m2m_chan->device->device_prep_slave_sg(dma_m2m_chan,sg2, 3, dma_m2m_config.direction, 0);
#else
    dma_m2m_desc = dma_m2m_chan->device->device_prep_dma_sg(dma_m2m_chan,sg2, 3, sg, 3, 0);
#endif

 

    dma_m2m_desc->callback = dma_m2m_callback;
    dmaengine_submit(dma_m2m_desc);
#if (LINUX_VERSION_CODE >= KERNEL_VERSION(3,0,35))
    dma_async_issue_pending(dma_m2m_chan);
#endif

 

    wait_for_completion(&dma_m2m_ok);
    dma_unmap_sg(NULL, sg, 3, dma_m2m_config.direction);
    dma_unmap_sg(NULL, sg2, 3, dma_m2m_config.direction);
#if (LINUX_VERSION_CODE >= KERNEL_VERSION(3,0,35))
    dma_src = dma_map_single(NULL, wbuf4, SDMA_BUF_SIZE, DMA_TO_DEVICE);
    dma_dst = dma_map_single(NULL, rbuf4, SDMA_BUF_SIZE, DMA_FROM_DEVICE);
    dma_m2m_desc = dma_m2m_chan->device->device_prep_dma_memcpy(dma_m2m_chan, dma_dst, dma_src, SDMA_BUF_SIZE,0);
    if (!dma_m2m_desc)
        printk("prep error!!\n");
    dma_m2m_desc->callback = dma_m2m_callback;
    dmaengine_submit(dma_m2m_desc);
    dma_async_issue_pending(dma_m2m_chan);
    wait_for_completion(&dma_m2m_ok);
    dma_unmap_single(NULL, dma_src, SDMA_BUF_SIZE, DMA_TO_DEVICE);
    dma_unmap_single(NULL, dma_dst, SDMA_BUF_SIZE, DMA_FROM_DEVICE);
#endif

 

    return 0;
}

 

struct file_operations dma_fops = {
    open:        sdma_open,
    release:    sdma_release,
    read:        sdma_read,
    write:        sdma_write,
};

 

int __init sdma_init_module(void)
{
#if (LINUX_VERSION_CODE >= KERNEL_VERSION(2,6,26))
    struct device *temp_class;
#else
    struct class_device *temp_class;
#endif
    int error;

 

    /* register a character device */
    error = register_chrdev(0, "sdma_test", &dma_fops);
    if (error < 0) {
        printk("SDMA test driver can't get major number\n");
        return error;
    }
    gMajor = error;
    printk("SDMA test major number = %d\n",gMajor);

 

    dma_tm_class = class_create(THIS_MODULE, "sdma_test");
    if (IS_ERR(dma_tm_class)) {
        printk(KERN_ERR "Error creating sdma test module class.\n");
        unregister_chrdev(gMajor, "sdma_test");
        return PTR_ERR(dma_tm_class);
    }

 

#if (LINUX_VERSION_CODE >= KERNEL_VERSION(2,6,28))
    temp_class = device_create(dma_tm_class, NULL,
                   MKDEV(gMajor, 0), NULL, "sdma_test");
#elif (LINUX_VERSION_CODE >= KERNEL_VERSION(2,6,26))
    temp_class = device_create(dma_tm_class, NULL,
                   MKDEV(gMajor, 0), "sdma_test");
#else
    temp_class = class_device_create(dma_tm_class, NULL,
                         MKDEV(gMajor, 0), NULL,
                         "sdma_test");
#endif
    if (IS_ERR(temp_class)) {
        printk(KERN_ERR "Error creating sdma test class device.\n");
        class_destroy(dma_tm_class);
        unregister_chrdev(gMajor, "sdma_test");
        return -1;
    }

 

    printk("SDMA test Driver Module loaded\n");
    return 0;
}

 

static void sdma_cleanup_module(void)
{
    unregister_chrdev(gMajor, "sdma_test");
#if (LINUX_VERSION_CODE >= KERNEL_VERSION(2,6,26))
    device_destroy(dma_tm_class, MKDEV(gMajor, 0));
#else
    class_device_destroy(dma_tm_class, MKDEV(gMajor, 0));
#endif
    class_destroy(dma_tm_class);

 

    printk("SDMA test Driver Module Unloaded\n");
}

 


module_init(sdma_init_module);
module_exit(sdma_cleanup_module);

 

MODULE_AUTHOR("Freescale Semiconductor");
MODULE_DESCRIPTION("SDMA test driver");
MODULE_LICENSE("GPL");

Original Attachment has been moved to: imx-sdma.c.zip

Original Attachment has been moved to: mxc_sdma_memcopy_test.c.zip

Labels (1)
0 Kudos
Reply
1 Reply

1,055 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sharp

one can check with official nxp L4.1.15

https://community.nxp.com/message/862063?commentID=862063#comment-862063 

sorry, L4.1.18 not officially supported by nxp, below link nxp bsp releases

i.MX 6 Series Software and Development Tool|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply