sdma compiler not find

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sdma compiler not find

1,748 Views
delauratfrançoi
Contributor II

Hello,

My name is françois, I work with imx6 dual and I would like to work with sdma core. I read  lot of documentation on subject . I seek a compiler but I don't find.

Can you help me please.

Thank you in advance for your reply

Best regards,

François.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,554 Views
ceggers1
Contributor IV

Hi François,

please see the following page for some of my SDMA tools. There is no compiler available (as the SDMA has not the necessary features for running compiled C code), but I wrote an assembler and a debugger.

https://community.nxp.com/t5/i-MX-Processors/SDMA-port-for-GNU-binutils-assembler-linker-debugger/m-...

regards
Christian

 

0 Kudos
Reply

1,603 Views
igorpadykov
NXP Employee
NXP Employee

HI François.

nxp does not support custom sdma scripts, so there are no officially provided sdma tools.

It may be useful to look at

http://billauer.co.il/blog/2011/10/imx-sdma-howto-memory-map/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply