sdma compiler not find

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sdma compiler not find

1,738件の閲覧回数
delauratfrançoi
Contributor II

Hello,

My name is françois, I work with imx6 dual and I would like to work with sdma core. I read  lot of documentation on subject . I seek a compiler but I don't find.

Can you help me please.

Thank you in advance for your reply

Best regards,

François.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,544件の閲覧回数
ceggers1
Contributor IV

Hi François,

please see the following page for some of my SDMA tools. There is no compiler available (as the SDMA has not the necessary features for running compiled C code), but I wrote an assembler and a debugger.

https://community.nxp.com/t5/i-MX-Processors/SDMA-port-for-GNU-binutils-assembler-linker-debugger/m-...

regards
Christian

 

0 件の賞賛
返信

1,593件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI François.

nxp does not support custom sdma scripts, so there are no officially provided sdma tools.

It may be useful to look at

http://billauer.co.il/blog/2011/10/imx-sdma-howto-memory-map/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信