run upgradeu is not working in U-Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

run upgradeu is not working in U-Boot

Jump to solution
3,711 Views
ashoksowndar
Contributor II

I have tried to update my U-Boot in my nitrogen 8m devices, but whenever i tried to execute the command in U-Boot it results in following error

Starting the controller
"USB XHCI 1.10
scanning bus 0 for devices... 1 USB Device(s) found
scanning bus 1 for devices... WARN halted endpoint, queueing URB anyway.
Unexpected XHCI event TRB, skipping... (bed3bab0 00000000 13000000 03008401)
BUG at drivers/usb/host/xhci-ring.c:495/abort_td()!
BUG!
resetting ..."

Please help me with this...

Regards,

Ashok S

0 Kudos
Reply
1 Solution
3,583 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ashok S,

The Nitrogen8M is manufactured and supported by Boundary Devices so I would recommend reaching to them for more information on features from their bootloader or BSP.

They have some documentation which may help or from where you can ask for further support:

https://boundarydevices.com/how-to-upgrade-u-boot/

My apologies for the inconvenience!

Regards,

View solution in original post

1 Reply
3,584 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ashok S,

The Nitrogen8M is manufactured and supported by Boundary Devices so I would recommend reaching to them for more information on features from their bootloader or BSP.

They have some documentation which may help or from where you can ask for further support:

https://boundarydevices.com/how-to-upgrade-u-boot/

My apologies for the inconvenience!

Regards,