run opencl app on iMX6Q: openCV error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

run opencl app on iMX6Q: openCV error

1,189件の閲覧回数
Gavin
Contributor I

we run the opencl test program(we want use GPU to accelate image processing speed) on the imx6q platform BSP Linux 3.14.52, and get the error infomation below(the same error happened in BSP Linux 4.1.15):
In image read [1520 x 932]
loops: 0, detect face using gpu...

OpenCV Error: Assertion failed (localThreads[0] * localThreads[1] * localThreads[2] <= kernelWorkGroupSize) in openCLVerifyKernel, file /home/tangb/yocto/imx-3.14.52-1.1.0_ga/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/opencv/2.4.11+gitAUTOINC+2c9547e314-r0/git/modules/ocl/src/cl_operations.cpp, line 349
terminate called after throwing an instance of 'cv::Exception'
what(): /home/tangb/yocto/imx-3.14.52-1.1.0_ga/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/opencv/2.4.11+gitAUTOINC+2c9547e314-r0/git/modules/ocl/src/cl_operations.cpp:349: error: (-215) localThreads[0] * localThreads[1] * localThreads[2] <= kernelWorkGroupSize in function openCLVerifyKernel

Aborted
root@imx6qsabresd:~#

And we test function is:

void detect( Mat& img, vector<Rect>& faces,
ocl::OclCascadeClassifier& cascade,
double scale, bool calTime)
{
printf("detect face using gpu...\n\n");
ocl::oclMat image(img);
ocl::oclMat gray, smallImg( cvRound (img.rows/scale), cvRound(img.cols/scale), CV_8UC1 );
if(calTime) workBegin();
ocl::cvtColor( image, gray, CV_BGR2GRAY );
ocl::resize( gray, smallImg, smallImg.size(), 0, 0, INTER_LINEAR );
ocl::equalizeHist( smallImg, smallImg );

cascade.detectMultiScale( smallImg, faces, 1.1,
3, 0
|CV_HAAR_SCALE_IMAGE
, Size(30,30), Size(0, 0) );
printf("#### 6\n");
printf("detect %d faces:\n",faces.size());
for(int i = 0;i < faces.size();i++){
printf("face %d : (%d,%d,%d,%d)\n",i,faces[i].x,faces[i].y,faces[i].width,faces[i].height);
}
if(calTime) workEnd();
}

someone can tell us how to do?

0 件の賞賛
返信
1 返信

956件の閲覧回数
b36401
NXP Employee
NXP Employee

Please look at this document regarding to face detection:
https://community.nxp.com/message/1026448

And this one is related to i.MX6:
http://imxcv.blogspot.com/2014/02/building-opencv-24x-for-freescales-imx6.html

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信