rt1180 program on flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

rt1180 program on flash

2,415件の閲覧回数
SimoneColomboWEG
Contributor III

Hi,

i've a weird problem on rt1180, if i make a new project on M33 with default config proposed by MCUXpresso, compile and download into flash the program works with no problem, print the default "Hello Word" correcty so all things are done with no problem.

If i do the same thing with a new project on M7 compile correcltly but when i try do debug this is the result:

LinkServer RedlinkMulti Driver v24.12 (Dec 18 2024 18:34:07 - crt_emu_cm_redlink build 869)

Found chip XML file in C:/Users/colombos/Documents/MCUXpressoIDE_24.12.148/workspace/MIMXRT1189_Project_m7/Debug\MIMXRT1189xxxxx.xml

Reconnected to existing LinkServer process.

============= SCRIPT: RT1180_connect_M33_wake_M7_ITC.scp =============

RT1180 Connect M33 and Wake M7 to ITC Script

DpID = 5BA02477

APID = 0x74770001

************ runBootLoader to enter serial downloader mode *************

PC = 1001BC6A, SP = 2001FFF4

DpID = 5BA02477

APID = 0x74770001

R15 = 0x1001C086

********** Initialize CM33 ************

Filling 0xE000E180 + 0x00000040 with 0xFFFFFFFF

Filling 0xE000E280 + 0x00000040 with 0xFFFFFFFF

Filling 0x201E0000 + 0x00020000 with 0x00000000

Filling 0x20200008 + 0x0001FFF8 with 0x00000000

************* Enable CM7 **************

************ Prepare Clock *************

******** Creating Landing Zone *********

Filling 0x303C0000 + 0x00020000 with 0x00000000

Filling 0x303E0000 + 0x00020000 with 0x00000000

Filling 0x30400000 + 0x00020000 with 0x00000000

Filling 0x30420000 + 0x00020000 with 0x00000000

************* Kickoff CM7 **************

Resp1 : 0xE1D20206

Resp2 : 0x000000D6

TAP 0: 5BA02477 AP 0: APID: 74770001 ROM Table: 00000002

TAP 0: 5BA02477 AP 1: APID: 44770002 ROM Table: 80000003

TAP 0: 5BA02477 Core 2: M7 APID: 74770001 ROM Table: E00FD003*

TAP 0: 5BA02477 Core 3: M33 APID: 74770001 ROM Table: E00FF003

APID = 0x74770001

============= END SCRIPT =============================================

Probe Firmware: MCU-LINK on-board (r1E2) CMSIS-DAP V3.153 (NXP Semiconductors)

Serial Number: OK1PG5OV03J1X

VID:PID: 1FC9:0143

USB Path: 0001:002a:00

Using memory from core 2 after searching for a good core

( 30) Emulator Connected

debug interface type = CoreSight DP (DAP DP ID 5BA02477) over SWD TAP 0

processor type = Cortex-M7 (CPU ID 00000C27) on DAP AP 2

number of h/w breakpoints = 8

number of flash patches = 0

number of h/w watchpoints = 4

Probe(0): Connected&Reset. DpID: 5BA02477. CpuID: 00000C27. Info: <None>

Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.

Content of CoreSight Debug ROM(s):

RBASE E00FD000: CID B105100D PID 000008E88C ROM (type 0x1)

ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM (type 0x1)

ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM (type 0x1)

ROM 3 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)

ROM 3 E0001000: CID B105E00D PID 04000BB002 Gen DWT (type 0x0)

ROM 3 E0002000: CID B105E00D PID 04000BB00E Gen (type 0x0)

ROM 3 E0000000: CID B105E00D PID 04000BB001 Gen ITM (type 0x0)

ROM 2 E0041000: CID B105900D PID 04001BB975 CSt ARM ETMv4.0 type 0x13 Trace Source - Core

ROM 2 E0042000: CID B105900D PID 04004BB906 CSt type 0x14 Debug Control - Trigger, e.g. ECT

ROM 1 E0043000: CID B105900D PID 04001BB908 CSt CSTF type 0x12 Trace Link - Trace funnel/router

CM7 Rev. 7.0 DTCM: 512KB ITCM: 512KB

LoUU: Level 2: LoC: Level 2

Level 1 Cache Type: Instruction+Data

ICache 32K: WT: Y WB: Y RA: Y WA: Y NumSets: 512 Assoc: 2 LineSize: 8

DCache 32K: WT: Y WB: Y RA: Y WA: Y NumSets: 256 Assoc: 4 LineSize: 8

NXP: MIMXRT1189xxxxx

Inspected v.2 External Flash Device on SPI using SFDP JEDEC ID MIMXRT1180_SFDP_FlexSPI1_A_QSPI.cfx

Image 'iMXRT1180_SFDP_FlexSPI1_A_QSPI Dec 18 2024 17:30:53'

Opening flash driver MIMXRT1180_SFDP_FlexSPI1_A_QSPI.cfx

Sending VECTRESET to run flash driver

AFTER driver startup timeout (302 5ms retries)

Driver Addresses

Start: 20000000

Entry: 2000009D

End: 2000075C

Stack: 20002760

Mailbox:2000A760

Driver Register State

R0: 00000000

R1: 00000000

R2: 00000000

R3: 00000000

R4: 2000A760

R5: 00000000

R6: 00000000

R7: 00000000

R8: 00000000

R9: 00000000

R10: 00000000

R11: 00000000

R12: 00000000

SP: 20002740

LR: FFFFFFF9 (exception from main thread)

PC: E7FEE7FE

xPSR: 40000003

MSP: 20002740

PSP: 20002760

CFBP: 00000001 (CONTROL=0x0, FAULTMASK=0x0, BASEPRI=0x0, PRIMASK=0x1)

Stacked Exception information at MSP

2000275C: xPSR: 41000000

20002758: VECTPC: 200000A2

20002754: LR: 2000009D

20002750: R12: 00000000

2000274C: R3: 00000000

20002748: R2: 00000000

20002744: R1: 00000000

20002740: R0: 00000000

Exception registers

E000ED04: ICSR: 00400803 (ISRPENDING, VECTPEND=0(none), RETTOBASE, VECTACTIVE=3(hard fault))

E000ED08: VTOR: 00000000 TBLBASE=0(INCODE), TBLOFF=0x0

E000ED28: MMFSR: 01 (IACCVIOL)

E000ED29: BFSR: 00

E000ED2A: UFSR: 0001 (UNDEFINSTR)

E000ED2C: HFSR: 40000000 (FORCED)

E000ED30: DFSR: 00000001 (HALTED)

E000ED3C: AFSR: 00000000

E000ED24: SHCSR: 00000000

E000ED34: MMAR: 00000000

E000ED38: BFAR: 00000000

E000EDFC: DEMCR: 01000000 (TRCENA)

VECTPC instructions near 41000000

40FFFFFC: (can't read - Nn(05). Wire ACK Fault in DAP access)

40FFFFFE: (can't read)

Flash Driver V.2 startup failed - rc Ef(34): Timed-out initializing flash.

chip initialization failed - Ef(34): Timed-out initializing flash.

failed to initialize flash driver MIMXRT1180_SFDP_FlexSPI1_A_QSPI.cfx

 

 

please help me to fix this issue.

 

i'm using MCUXpresso 24.12 build 148 and SDK 24.12.00 then i've just tried to update MCU-Link to version 3.153

 

the demoboard is:

SCH-5077 REV C3

700-5077 REV C1(is signed with a point with pen)

Simone

0 件の賞賛
返信
2 返答(返信)

2,400件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello, I hope you are well. 

RT1180 is a product in pre-production, please contact your NXP representative for more detailed information. 

Best regards,
Omar

0 件の賞賛
返信

2,412件の閲覧回数
SimoneColomboWEG
Contributor III

if needed the projects

0 件の賞賛
返信