rt1170 jlink issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

rt1170 jlink issue

Jump to solution
1,726 Views
sukyeong
Contributor III

MCU : IMXRT1170-EVB

J-LINK , i want to use JTAG mode

swd mode works fine, but jtag mode is error.

I've referred to the posts below, but it doesn't work out.

help me please

 

https://community.nxp.com/t5/i-MX-RT/RT1176-connect-to-JLINK-with-a-warning/m-p/1599341

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-J-Link-with-MIMXRT1160-EVK-or-MIMXRT1170-E...

 

sukyeong_0-1686792722753.png

1. i try j6,j7 jumper remove

2. Is there anything in the circuit that needs to be changed?

sukyeong_1-1686792812321.png

sukyeong_2-1686792840297.png

 

0 Kudos
Reply
1 Solution
1,643 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

By default, the RT1170 silicon can use both SWD and JTAG modes using the Arm stitching sequence. For the RT1170EVK board, it defaults to use the SWD debug without any board modification. If you want to use the JTAG debug, solder out R187, R208, R195, and R78, because some JTAG signals are multiplexed with other functions.

 

Regards,

Jing

View solution in original post

7 Replies
1,702 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

Please try to remove R2152 and  R2038.

 

Regards,

Jing

0 Kudos
Reply
1,698 Views
sukyeong
Contributor III

R2152, R2038을 찾을 수 없습니다..
자세한 내용을 알려주실 수 있나요?

 

@jingpan 

Tags (1)
0 Kudos
Reply
1,675 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

You can search to this doc.

0 Kudos
Reply
1,666 Views
sukyeong
Contributor III
0 Kudos
Reply
1,663 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

What is your board, EVK or EVKB?

 

Regards,

Jing

0 Kudos
Reply
1,657 Views
sukyeong
Contributor III
My board is EVK.
sorry for the confusion
@jingpan
0 Kudos
Reply
1,644 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

By default, the RT1170 silicon can use both SWD and JTAG modes using the Arm stitching sequence. For the RT1170EVK board, it defaults to use the SWD debug without any board modification. If you want to use the JTAG debug, solder out R187, R208, R195, and R78, because some JTAG signals are multiplexed with other functions.

 

Regards,

Jing