rootfs no linuxrc file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

rootfs no linuxrc file

1,542 Views
fulinux
Contributor IV

Hi,

i use imx-4.1.15-1.0.0_ga bsp create fsl-image-qt5-imx6qsabresd-20160511030807.rootfs.tar.bz2 roofs file, but there is no linuxrc init file in root directory, what should i set init option for bootargs?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,451 Views
b36401
NXP Employee
NXP Employee

Actually our image does not use such init file as linuxrc.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply