roadmap meta-imx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

roadmap meta-imx

2,773 Views
Jeroen_H
Contributor III

Hi !

We are planning to upgrade our Yocto build environment.

Currently, the meta-imx layer is available for Zeus and Hardknott.

Are there any plans to update the BSP meta-imx to Honister and/or Kirkstone? 
Is there a roadmap for this somewhere with estimated release dates?

Thank you very much.

Jeroen.

Labels (1)
Tags (2)
0 Kudos
Reply
4 Replies

2,269 Views
fenil
Contributor I

Hi, is there a plan to upgrade the BSP to Kirkstone in near future ?
Since honister support will not be available post MAY-2022. 

0 Kudos
Reply

2,752 Views
Jeroen_H
Contributor III

Hi Igor, 

Thanks for answering!
Do you have contact details of the local marketing office in Europe so I can contact them ?


Kind regards,
Jeroen.

0 Kudos
Reply

2,750 Views
igorpadykov
NXP Employee
NXP Employee

local NXP Sales Offices:


http://www.nxp.com/about/about-nxp/worldwide-locations:GLOBAL_SITES

 

Best regards
igor

0 Kudos
Reply

2,756 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeroen

 

yes there plans to update the BSP to Honister in next year, more detailed information

can be obtained from local marketing office.

 

Best regards
igor