MMC init failed while rebooting i.mx6ull

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMC init failed while rebooting i.mx6ull

1,256件の閲覧回数
nikhilmm
Contributor I

Hi,

MMC init is failing in uboot, when reboot is done by software.

Logs are as follows,

Rebooting... reboot: Restarting system

U-Boot 2016.03-g0365239-dirty (Sep 14 2021 - 12:25:51 +0530)

CPU: Freescale i.MX6ULL rev1.1 528 MHz (running at 396 MHz)
CPU: Commercial temperature grade (0C to 95C) at 46C
Reset cause: POR
u-boot revision: 9.00.04 compiled on 20-July-2021
I2C: ready
DRAM: 512 MiB
board_init
MMC: board_mmc_init
FSL_SDHC: 0, FSL_SDHC: 1
board_mmc_getcd
MMC: no card present
*** Warning - MMC init failed, using default environment

 

**********do_enable_parallel_lcd*****************
Display: TFT43AB (1024x600)
Video: 1024x600x24
CONFIG_SPLASH_SCREEN
In CONFIG_SPLASH_SCREEN_ALIGN
In CONFIG_SPLASH_SCREEN_ALIGN
CONFIG_SPLASH_SCREEN_ALIGN
In: serial
Out: serial
Err: serial
board_late_init
Net: FEC1
Error: FEC1 address not set.

 

Normal Boot
Hit any key to stop autoboot: 0
board_mmc_getcd
MMC: no card present
board_mmc_getcd
MMC: no card present
board_mmc_getcd
MMC: no card present
board_mmc_getcd
MMC: no card present
board_mmc_getcd
MMC: no card present
Not valid image format for Authentication, Please check

ラベル(4)
0 件の賞賛
返信
0 返答(返信)