"random: systemd: uninitialized urandom read" systemd issue in new BSP imx-5.4.24-2.1.0.xml

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"random: systemd: uninitialized urandom read" systemd issue in new BSP imx-5.4.24-2.1.0.xml

4,469 Views
rakesh_patel
Senior Contributor I

Board:

===========

imx6sx

 

Issue log

==============

1.837669] systemd[1]: Set hostname to <imx6sxsabresd>.
[ 2.426892] random: systemd: uninitialized urandom read (16 bytes read)
[ 2.434933] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.

 

Query:

===========

1) why "random: systemd: uninitialized urandom read" comes? And how to solve it?

 

Labels (1)
0 Kudos
Reply
6 Replies

4,462 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello rakesh_patel,

 

You need to recompile your yocto again or it is a bad download of the image since the error never happend with the EVK. Probably there is problem with your Kernel configuration file. Or see othe possible solution on google, but this erros never happend on MX6SX.

 

Regards

 

0 Kudos
Reply

4,459 Views
rakesh_patel
Senior Contributor I

@Bio_TICFSL :

Here are the logs from imx6sx EVK as well with prebuilt binaries:

======================================

Welcome to NXP i.MX Release Distro 5.4-zeus (zeus)!
[    4.533441] systemd[1]: Set hostname to <imx6qpdlsolox>.
[    4.548971] random: systemd: uninitialized urandom read (16 bytes read)
[    4.556032] systemd[1]: Initializing machine ID from random generator.
[    5.042508] systemd[1]: /lib/systemd/system/dbus.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/dbus
/system_bus_socket ��→ /run/dbus/system_bus_socket; please update the unit file accordingly.
[    5.078463] systemd[1]: /lib/systemd/system/syslogd.service:8: PIDFile= references a path below legacy directory /var/run/, updating /var/run/syslo
gd.pid ��→ /run/syslogd.pid; please update the unit file accordingly.
[    5.123836] systemd[1]: /lib/systemd/system/rpcbind.socket:5: ListenStream
 
 
Query:
===========
1) Do you have idea for how to resolve this?
0 Kudos
Reply

4,447 Views
rakesh_patel
Senior Contributor I

@Bio_TICFSL :

Any update here?

0 Kudos
Reply

4,428 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Does this happens with other kernel? I can not see in 5.4.24 but i wonder if this happens to you with other kernel.

 

Regards

 

0 Kudos
Reply

4,425 Views
rakesh_patel
Senior Contributor I

@Bio_TICFSL :

Are you sure that "I can not see in 5.4.24".

I have also checked with NXP's prebuilt binaries. The same issue is there.

 

Can you please share your logs where this error is not faced?

 

0 Kudos
Reply

4,446 Views
rakesh_patel
Senior Contributor I

@igorpadykov :

Do you have any idea for this issue?

0 Kudos
Reply