"random: systemd: uninitialized urandom read" systemd issue in new BSP imx-5.4.24-2.1.0.xml

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

"random: systemd: uninitialized urandom read" systemd issue in new BSP imx-5.4.24-2.1.0.xml

4,482 次查看
rakesh_patel
Senior Contributor I

Board:

===========

imx6sx

 

Issue log

==============

1.837669] systemd[1]: Set hostname to <imx6sxsabresd>.
[ 2.426892] random: systemd: uninitialized urandom read (16 bytes read)
[ 2.434933] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.

 

Query:

===========

1) why "random: systemd: uninitialized urandom read" comes? And how to solve it?

 

标签 (1)
0 项奖励
回复
6 回复数

4,475 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello rakesh_patel,

 

You need to recompile your yocto again or it is a bad download of the image since the error never happend with the EVK. Probably there is problem with your Kernel configuration file. Or see othe possible solution on google, but this erros never happend on MX6SX.

 

Regards

 

0 项奖励
回复

4,472 次查看
rakesh_patel
Senior Contributor I

@Bio_TICFSL :

Here are the logs from imx6sx EVK as well with prebuilt binaries:

======================================

Welcome to NXP i.MX Release Distro 5.4-zeus (zeus)!
[    4.533441] systemd[1]: Set hostname to <imx6qpdlsolox>.
[    4.548971] random: systemd: uninitialized urandom read (16 bytes read)
[    4.556032] systemd[1]: Initializing machine ID from random generator.
[    5.042508] systemd[1]: /lib/systemd/system/dbus.socket:5: ListenStream= references a path below legacy directory /var/run/, updating /var/run/dbus
/system_bus_socket ��→ /run/dbus/system_bus_socket; please update the unit file accordingly.
[    5.078463] systemd[1]: /lib/systemd/system/syslogd.service:8: PIDFile= references a path below legacy directory /var/run/, updating /var/run/syslo
gd.pid ��→ /run/syslogd.pid; please update the unit file accordingly.
[    5.123836] systemd[1]: /lib/systemd/system/rpcbind.socket:5: ListenStream
 
 
Query:
===========
1) Do you have idea for how to resolve this?
0 项奖励
回复

4,460 次查看
rakesh_patel
Senior Contributor I

@Bio_TICFSL :

Any update here?

0 项奖励
回复

4,441 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Does this happens with other kernel? I can not see in 5.4.24 but i wonder if this happens to you with other kernel.

 

Regards

 

0 项奖励
回复

4,438 次查看
rakesh_patel
Senior Contributor I

@Bio_TICFSL :

Are you sure that "I can not see in 5.4.24".

I have also checked with NXP's prebuilt binaries. The same issue is there.

 

Can you please share your logs where this error is not faced?

 

0 项奖励
回复

4,459 次查看
rakesh_patel
Senior Contributor I

@igorpadykov :

Do you have any idea for this issue?

0 项奖励
回复