"programming algorithm" in KEILMDK -> Utilities tab for NXP MIMXRT1170-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"programming algorithm" in KEILMDK -> Utilities tab for NXP MIMXRT1170-EVK

ソリューションへジャンプ
1,831件の閲覧回数
SakSath
Contributor III

Hi,

I am trying to flash a demo application built on KEIL MDK on to MIMXRT1170-EVK.

However I am currently facing the below issue:


SakSath_0-1659938155838.png

I am new to NXP MIMXRT1170-EVK and after initial search about the issue I am facing I see some suggestions to change the "Programming algorithm".

However, I find little information about this in the getting started guide of the board.

Can You please help with the appropriate settings for successful flash and debugging?

0 件の賞賛
返信
1 解決策
1,820件の閲覧回数
SakSath
Contributor III

Hi @jay_heng ,

Thanks!

I was able to resolve the flashing issue with the help of settings from another demo project. I will close this post.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,828件の閲覧回数
jay_heng
NXP Employee
NXP Employee

You can refer to below blog (it is in Chinese)

https://www.cnblogs.com/henjay724/p/15465655.html

1,821件の閲覧回数
SakSath
Contributor III

Hi @jay_heng ,

Thanks!

I was able to resolve the flashing issue with the help of settings from another demo project. I will close this post.

0 件の賞賛
返信