"programming algorithm" in KEILMDK -> Utilities tab for NXP MIMXRT1170-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"programming algorithm" in KEILMDK -> Utilities tab for NXP MIMXRT1170-EVK

Jump to solution
1,835 Views
SakSath
Contributor III

Hi,

I am trying to flash a demo application built on KEIL MDK on to MIMXRT1170-EVK.

However I am currently facing the below issue:


SakSath_0-1659938155838.png

I am new to NXP MIMXRT1170-EVK and after initial search about the issue I am facing I see some suggestions to change the "Programming algorithm".

However, I find little information about this in the getting started guide of the board.

Can You please help with the appropriate settings for successful flash and debugging?

0 Kudos
Reply
1 Solution
1,824 Views
SakSath
Contributor III

Hi @jay_heng ,

Thanks!

I was able to resolve the flashing issue with the help of settings from another demo project. I will close this post.

View solution in original post

0 Kudos
Reply
2 Replies
1,832 Views
jay_heng
NXP Employee
NXP Employee

You can refer to below blog (it is in Chinese)

https://www.cnblogs.com/henjay724/p/15465655.html

1,825 Views
SakSath
Contributor III

Hi @jay_heng ,

Thanks!

I was able to resolve the flashing issue with the help of settings from another demo project. I will close this post.

0 Kudos
Reply