when the board is hot, it happened to vpu blocking, logs as following,
and the issue still existed after rebooting.
Is is related to temperature?
U-Boot 2009.08 (Jun 12 2016 - 10:45:30)
CPU: Freescale i.MX6 family TO1.5 at 792 MHz
Thermal sensor with ratio = 178
Temperature: 58 C, calibration data 0x5684d769
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63015 [POR ]
Boot Device: SD
I2C: ready
DRAM: 2 GB
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2
*** Warning - bad CRC or MMC, using default environment
In: serial
Out: serial
Err: serial
Found PFUZE100! deviceid=10,revid=21
Net: No ethernet found.
hw version:1
Hit any key to stop autoboot: 0
kernel @ 10808000 (4734496)
ramdisk @ 11800000 (1838792)
kernel cmdline:
use boot.img command line:
console=ttymxc1,115200 init=/init video=mxcfb0:dev=ldb,LDB-WSVGA,if=RGB24,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc1 androidboot.hardware=freescale maxcpus=4 no_console_suspend=1 androidboot.serialno=121a11d4e315dec4 hw_rev=1
Starting kernel ...
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Linux version 3.0.35-00003-g041d520 (kris@ecovacs) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #284 SMP PREEMPT Tue Jun 21 11:11:58 CST 2016
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board
[ 0.000000] Ignoring unrecognised tag 0x54410008
[ 0.000000] hw_rev:1
[ 0.000000] Memory policy: ECC disabled, Data cache writealloc
[ 0.000000] CPU identified as i.MX6Q, unknown revision
[ 0.000000] PERCPU: Embedded 7 pages/cpu @c29ce000 s6528 r8192 d13952 u32768
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 468224
[ 0.000000] Kernel command line: console=ttymxc1,115200 init=/init video=mxcfb0:dev=ldb,LDB-WSVGA,if=RGB24,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc1 androidboot.hardware=freescale maxcpus=4 no_console_suspend=1 androidboot.serialno=121a11d4e315dec4 hw_rev=1
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 379MB 378MB 848MB 240MB = 1845MB total
[ 0.000000] Memory: 1859580k/1859580k available, 237572k reserved, 1489920K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xfbe00000 - 0xffe00000 ( 64 MB)
[ 0.000000] vmalloc : 0xd9800000 - 0xf2000000 ( 392 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd9000000 ( 400 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .init : 0xc0008000 - 0xc0046000 ( 248 kB)
[ 0.000000] .text : 0xc0046000 - 0xc08aa534 (8594 kB)
[ 0.000000] .data : 0xc08ac000 - 0xc0927258 ( 493 kB)
[ 0.000000] .bss : 0xc092727c - 0xc0aaf5bc (1569 kB)
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] NR_IRQS:624
[ 0.000000] MXC GPIO hardware
[ 0.000000] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
[ 0.000000] arm_max_freq=1GHz
[ 0.000000] MXC_Early serial console at MMIO 0x21e8000 (options '115200')
[ 0.000000] bootconsole [ttymxc1] enabled
[ 0.235636] Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
[ 0.328369] pid_max: default: 32768 minimum: 301
[ 0.333157] Security Framework initialized
[ 0.337313] SELinux: Initializing.
[ 0.340956] Mount-cache hash table entries: 512
[ 0.346267] Initializing cgroup subsys debug
[ 0.350592] Initializing cgroup subsys cpuacct
[ 0.355097] Initializing cgroup subsys freezer
[ 0.359589] CPU: Testing write buffer coherency: ok
[ 0.364800] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
[ 0.485464] CPU1: Booted secondary processor
[ 0.585473] CPU2: Booted secondary processor
[ 0.685452] CPU3: Booted secondary processor
[ 0.744794] Brought up 4 CPUs
[ 0.760620] SMP: Total of 4 processors activated (6324.22 BogoMIPS).
[ 0.790615] print_constraints: dummy:
[ 0.794633] NET: Registered protocol family 16
[ 0.804496] print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal
[ 0.812052] print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal
[ 0.819891] print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal
[ 0.827626] print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal
[ 0.835441] print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal
[ 0.843165] print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal
[ 0.853727] ram_console: got buffer at 3ff00000, size 100000
[ 0.859585] ram_console: uncorrectable error in header
[ 0.864742] ram_console: no valid data in buffer (sig = 0xc68c0ce3)
[ 0.877849] console [ram-1] enabled
[ 1.051050] hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
[ 1.058037] hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
[ 1.065476] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 1.071501] L310 cache controller enabled
[ 1.075622] l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B
[ 1.119271] bio: create slab <bio-0> at 0
[ 1.127648] mxs-dma mxs-dma-apbh: initialized
[ 1.132543] print_constraints: vmmc: 3300 mV
[ 1.137871] vgaarb: loaded
[ 1.141884] SCSI subsystem initialized
[ 1.146721] usbcore: registered new interface driver usbfs
[ 1.152459] usbcore: registered new interface driver hub
[ 1.158115] usbcore: registered new device driver usb
[ 1.163266] Freescale USB OTG Driver loaded, $Revision: 1.55 $
[ 1.176082] mc_pfuze 1-0008: ID: 0,Full lay: 2 ,Metal lay: 1
[ 1.184113] mc_pfuze 1-0008: FAB: 0 ,FIN: 0
[ 1.204432] pfuze100_init:Revision ID:21,arm_max_freq=2,enable_ldo_mode=1
[ 1.241124] pfuze100 init: set SWBST-----------==========>
[ 1.252947] print_constraints: PFUZE100_SW1A: 300 <--> 1875 mV at 1300 mV
[ 1.262456] print_constraints: PFUZE100_SW1B: 300 <--> 1875 mV at 300 mV
[ 1.275686] print_constraints: PFUZE100_SW1C: 300 <--> 1875 mV at 1300 mV
[ 1.285128] print_constraints: PFUZE100_SW2: 800 <--> 3950 mV at 3300 mV
[ 1.294522] print_constraints: PFUZE100_SW3A: 400 <--> 1975 mV at 1500 mV
[ 1.303958] print_constraints: PFUZE100_SW3B: 400 <--> 1975 mV at 1500 mV
[ 1.313474] print_constraints: PFUZE100_SW4: 800 <--> 3950 mV at 3150 mV
[ 1.322931] print_constraints: PFUZE100_SWBST: 5000 <--> 5150 mV at 5000 mV
[ 1.332534] print_constraints: PFUZE100_VSNVS: 1200 <--> 3000 mV at 1800 mV
[ 1.343812] print_constraints: PFUZE100_VREFDDR: at 750 mV
[ 1.351930] print_constraints: PFUZE100_VGEN1: 800 <--> 1550 mV at 1500 mV
[ 1.361502] print_constraints: PFUZE100_VGEN2: 800 <--> 1550 mV at 1500 mV
[ 1.371088] print_constraints: PFUZE100_VGEN3: 1800 <--> 3300 mV at 2800 mV
[ 1.384495] print_constraints: PFUZE100_VGEN4: 1800 <--> 3300 mV at 1800 mV
[ 1.397984] print_constraints: PFUZE100_VGEN5: 1800 <--> 3300 mV at 3000 mV
[ 1.407660] print_constraints: PFUZE100_VGEN6: 1800 <--> 3300 mV at 3300 mV
[ 1.434876] imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 1.442986] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 1.450473] Bluetooth: Core ver 2.16
[ 1.454372] NET: Registered protocol family 31
[ 1.458928] Bluetooth: HCI device and connection manager initialized
[ 1.465456] Bluetooth: HCI socket layer initialized
[ 1.470430] Bluetooth: L2CAP socket layer initialized
[ 1.475606] Bluetooth: SCO socket layer initialized
[ 1.481027] i2c-core: driver [max17135] using legacy suspend method
[ 1.487406] i2c-core: driver [max17135] using legacy resume method
[ 1.493770] Switching to clocksource mxc_timer1
[ 1.511573] NET: Registered protocol family 2
[ 1.516265] IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 1.523921] TCP established hash table entries: 65536 (order: 7, 524288 bytes)
[ 1.532338] TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
[ 1.540231] TCP: Hash tables configured (established 65536 bind 65536)
[ 1.546852] TCP reno registered
[ 1.550169] UDP hash table entries: 256 (order: 1, 8192 bytes)
[ 1.556108] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
[ 1.562933] NET: Registered protocol family 1
[ 1.567762] RPC: Registered named UNIX socket transport module.
[ 1.573807] RPC: Registered udp transport module.
[ 1.578691] RPC: Registered tcp transport module.
[ 1.583484] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.590103] PCI: CLS 0 bytes, default 32
[ 1.594295] Unpacking initramfs...
[ 1.717418] Freeing initrd memory: 1792K
[ 1.722472] PMU: registered new PMU device of type 0
[ 1.727666] Static Power Management for Freescale i.MX6
[ 1.733155] wait mode is enabled for i.MX6
[ 1.737542] cpaddr = d9880000 suspend_iram_base=d98fc000
[ 1.743118] PM driver module loaded
[ 1.747126] IMX usb wakeup probe
[ 1.750560] the wakeup pdata is 0xd41c96e0
[ 1.755211] add wake up source irq 75
[ 1.765626] IMX usb wakeup probe
[ 1.769053] the wakeup pdata is 0xd41c94a0
[ 1.773850] cpu regulator mode:ldo_bypass
[ 1.786210] _regulator_get: get() with no identifier
[ 1.791285] mx6_cpu_regulator_init: failed to get pu regulator
[ 1.805621] i.MXC CPU frequency driver
[ 1.810080] audit: initializing netlink socket (disabled)
[ 1.815647] type=2000 audit(1.570:1): initialized
[ 1.842286] highmem bounce pool size: 64 pages
[ 1.847073] ashmem: initialized
[ 1.851536] NTFS driver 2.1.30 [Flags: R/O].
[ 1.855988] JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 1.862400] fuse init (API version 7.16)
[ 1.866626] msgmni has been set to 725
[ 1.870494] SELinux: Registering netfilter hooks
[ 1.876828] NET: Registered protocol family 38
[ 1.881542] cryptodev: driver loaded.
[ 1.885297] io scheduler noop registered
[ 1.889371] io scheduler deadline registered
[ 1.893771] io scheduler cfq registered (default)
[ 1.899987] MIPI DSI driver module loaded
[ 1.904257] mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb
[ 1.910726] _regulator_get: get() with no identifier
[ 1.917923] mxc_sdc_fb mxc_sdc_fb.1: Can't get fb option for mxcfb1!
[ 1.924381] imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00100000
[ 1.931695] mxc_sdc_fb mxc_sdc_fb.2: Can't get fb option for mxcfb2!
[ 1.938197] mxc_sdc_fb mxc_sdc_fb.3: Can't get fb option for mxcfb3!
[ 1.945233] imx-sdma imx-sdma: loaded firmware 1.1
[ 1.955290] imx-sdma imx-sdma: initialized
[ 2.086295] Serial: IMX driver
[ 2.089573] imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
[ 2.096530] imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX
[ 2.103095] console [ttymxc1] enabled, bootconsole disabled
[ 2.103095] console [ttymxc1] enabled, bootconsole disabled
[ 2.114742] imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
[ 2.121633] imx-uart.3: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX
[ 2.136916] loop: module loaded
[ 2.140217] at24 2-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write
[ 2.147474] xmf10411_i2c_probe
[ 2.150762] ks103_us_probe
[ 2.153537] ks103-ultrasonic 1-0073: I2C Address: 0x73
[ 2.159481] ks103-ultrasonic 1-0073: Write to device fails status fffffffb
[ 2.166423] ks103-ultrasonic 1-0073: Read year failed. ret:-5
[ 2.172303] ks103-ultrasonic 1-0073: Read version failed:-5
[ 2.177948] ks103-ultrasonic: probe of 1-0073 failed with error -5
[ 2.184269] ks103_us_probe
[ 2.187040] ks103-ultrasonic 1-0074: I2C Address: 0x74
[ 2.192963] ks103-ultrasonic 1-0074: Write to device fails status fffffffb
[ 2.199917] ks103-ultrasonic 1-0074: Read year failed. ret:-5
[ 2.205784] ks103-ultrasonic 1-0074: Read version failed:-5
[ 2.211438] ks103-ultrasonic: probe of 1-0074 failed with error -5
[ 2.217746] ks103_us_probe
[ 2.220531] ks103-ultrasonic 1-0075: I2C Address: 0x75
[ 2.226492] ks103-ultrasonic 1-0075: Write to device fails status fffffffb
[ 2.233455] ks103-ultrasonic 1-0075: Read year failed. ret:-5
[ 2.239332] ks103-ultrasonic 1-0075: Read version failed:-5
[ 2.244974] ks103-ultrasonic: probe of 1-0075 failed with error -5
[ 2.253147] GPMI NAND driver registered. (IMX)
[ 2.258690] vcan: Virtual CAN interface driver
[ 2.263211] CAN device driver interface
[ 2.267162] flexcan netdevice driver
[ 2.270994] FEC Ethernet Driver
[ 2.274355] PPP generic driver version 2.4.2
[ 2.279126] PPP Deflate Compression module registered
[ 2.284244] PPP BSD Compression module registered
[ 2.289559] PPP MPPE Compression module registered
[ 2.294418] NET: Registered protocol family 24
[ 2.298967] tun: Universal TUN/TAP device driver, 1.6
[ 2.304138] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
[ 2.310953] usbcore: registered new interface driver asix
[ 2.316604] usbcore: registered new interface driver cdc_ether
[ 2.322654] usbcore: registered new interface driver cdc_eem
[ 2.328583] usbcore: registered new interface driver dm9601
[ 2.334355] usbcore: registered new interface driver net1080
[ 2.340288] usbcore: registered new interface driver cdc_subset
[ 2.346409] usbcore: registered new interface driver zaurus
[ 2.352126] cdc_ncm: 04-Aug-2011
[ 2.355551] usbcore: registered new interface driver cdc_ncm
[ 2.361356] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.368109] fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
[ 2.374874] fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
[ 2.408475] fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
[ 2.428465] fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
[ 2.434752] hub 1-0:1.0: USB hub found
[ 2.438650] hub 1-0:1.0: 1 port detected
[ 2.442837] add wake up source irq 72
[ 2.446601] fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
[ 2.453365] fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
[ 2.488470] fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200
[ 2.508459] fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
[ 2.514780] hub 2-0:1.0: USB hub found
[ 2.518623] hub 2-0:1.0: 1 port detected
[ 2.523019] Initializing USB Mass Storage driver...
[ 2.528188] usbcore: registered new interface driver usb-storage
[ 2.534276] USB Mass Storage support registered.
[ 2.539023] ARC USBOTG Device Controller driver (1 August 2005)
[ 2.548317] android_usb gadget: Mass Storage Function, version: 2009/09/11
[ 2.555337] android_usb gadget: Number of LUNs=1
[ 2.560034] lun0: LUN: removable file: (no medium)
[ 2.565558] Gadget Android: controller 'fsl-usb2-udc' not recognized
[ 2.572004] android_usb gadget: android_usb ready
[ 2.576823] Suspend udc for OTG auto detect
[ 2.581087] USB Host suspend begins
[ 2.584638] will suspend roothub and its children
[ 2.589483] ehci_fsl_bus_suspend begins, DR
[ 2.593744] ehci_fsl_bus_suspend ends, DR
[ 2.597823] host suspend ends
[ 2.600923] USB Gadget resume begins
[ 2.604561] fsl_udc_resume, Wait for wakeup thread finishes
[ 2.613479] dr_controller_run: udc enter low power mode
[ 2.618873] USB Gadget resume ends
[ 2.622337] fsl-usb2-udc: bind to driver android_usb
[ 2.627947] mousedev: PS/2 mouse device common for all mice
[ 2.634111] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[ 2.663185] gt911-touch 2-0014: i2c test failed attempt 1: -5
[ 2.689116] gt911-touch 2-0014: i2c test failed attempt 2: -5
[ 2.718480] gt911-touch 2-0014: I2C communication failure: -5
[ 2.724298] gt911-touch: probe of 2-0014 failed with error -5
[ 2.787536] ft5x06-touch 2-0038: IC Version:0xa6
[ 2.792471] input: FocalTech Capacitive TouchScreen as /devices/virtual/input/input1
[ 2.801341] i2c-core: driver [isl29023] using legacy suspend method
[ 2.807726] i2c-core: driver [isl29023] using legacy resume method
[ 2.815215] using rtc device, snvs_rtc, for alarms
[ 2.819943] snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
[ 2.826986] i2c /dev entries driver
[ 2.831368] Linux video capture interface: v2.00
[ 2.838504] usb 2-1: new high speed USB device number 2 using fsl-ehci
[ 2.989923] hub 2-1:1.0: USB hub found
[ 2.993968] hub 2-1:1.0: 4 ports detected
[ 3.278729] usb 2-1.1: new high speed USB device number 3 using fsl-ehci
[ 3.358674] USB Gadget resume begins
[ 3.362316] fsl_udc_resume, Wait for wakeup thread finishes
[ 3.538612] usb 2-1.2: new high speed USB device number 4 using fsl-ehci
[ 5.884007] ov10635_set_regs ok
[ 5.892713] ov10635 0-0030: ov10635 Product ID a6 Manufacturer ID 35
[ 5.899207] ov10635 probe end
[ 5.902838] mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
[ 5.910602] mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
[ 5.918284] uvcvideo: Found UVC 1.00 device USB 2.0 Camera (0c45:62f1)
[ 5.930324] input: USB 2.0 Camera as /devices/platform/fsl-ehci.1/usb2/2-1/2-1.1/2-1.1:1.0/input/input2
[ 5.940270] usbcore: registered new interface driver uvcvideo
[ 5.946082] USB Video Class driver (v1.1.0)
[ 5.951003] i2c-core: driver [mag3110] using legacy suspend method
[ 5.957251] i2c-core: driver [mag3110] using legacy resume method
[ 5.963957] imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
[ 5.972363] device-mapper: uevent: version 1.0.3
[ 5.977328] device-mapper: ioctl: 4.20.0-ioctl (2011-02-02) initialised: dm-devel@redhat.com
[ 5.985934] Bluetooth: Virtual HCI driver ver 1.3
[ 5.990940] Bluetooth: HCI UART driver ver 2.2
[ 5.995452] Bluetooth: HCIATH3K protocol initialized
[ 6.000550] Bluetooth: Generic Bluetooth USB driver ver 0.6
[ 6.006356] usbcore: registered new interface driver btusb
[ 6.012372] sdhci: Secure Digital Host Controller Interface driver
[ 6.018635] sdhci: Copyright(c) Pierre Ossman
[ 6.023201] sdhci sdhci-esdhc-imx.2: no card-detect pin available!
[ 6.029768] mmc0: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA
[ 6.036984] sdhci sdhci-esdhc-imx.3: no write-protect pin available!
[ 6.046814] mmc1: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA
[ 6.053999] sdhci sdhci-esdhc-imx.1: no write-protect pin available!
[ 6.060489] sdhci sdhci-esdhc-imx.1: no card-detect pin available!
[ 6.074034] mmc2: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA
[ 6.081452] mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[ 6.093725] VPU initialized
[ 6.101737] mxc_asrc registered
[ 6.105126] Galcore version 4.6.9.9754
[ 6.139893] Thermal calibration data is 0x5684d769
[ 6.144807] Thermal sensor with ratio = 178
[ 6.168456] Anatop Thermal registered as thermal_zone0
[ 6.173898] anatop_thermal_probe: default cooling device is cpufreq!
[ 6.181910] usbcore: registered new interface driver usbhid
[ 6.187602] usbhid: USB HID core driver
[ 6.192086] logger: created 256K log 'log_main'
[ 6.196907] logger: created 256K log 'log_events'
[ 6.201988] logger: created 256K log 'log_radio'
[ 6.206909] logger: created 256K log 'log_system'
[ 6.210616] mmc0: new high speed SDHC card at address aaaa
[ 6.211074] mmcblk0: mmc0:aaaa SS08G 7.40 GiB
[ 6.216478] mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
[ 6.216765] mmcblk0: p4 size 13352010 extends beyond EOD, truncated
[ 6.368864] AIC3254: programming mini dsp
[ 6.372945] The register sections found in pps header file:
[ 6.378598] miniDSP_A_reg_values
[ 6.381941] miniDSP_D_reg_values
[ 6.385234] Registered minidsp driver, Major number: 247
[ 6.393212] asoc: tlv320aic32x4-hifi <-> imx-ssi.1 mapping ok
[ 6.400073] ALSA device list:
[ 6.403115] #0: aic3254-audio
[ 6.406721] oprofile: using arm/armv7-ca9
[ 6.411271] u32 classifier
[ 6.414044] Actions configured
[ 6.417508] Netfilter messages via NETLINK v0.30.
[ 6.422527] nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
[ 6.432871] ctnetlink v0.93: registering with nfnetlink.
[ 6.438333] NF_TPROXY: Transparent proxy support initialized, version 4.1.0
[ 6.445391] NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
[ 6.453763] xt_time: kernel timezone is -0000
[ 6.458309] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 6.463913] arp_tables: (C) 2002 David S. Miller
[ 6.468654] TCP cubic registered
[ 6.471946] Initializing XFRM netlink socket
[ 6.476717] NET: Registered protocol family 10
[ 6.481944] Mobile IPv6
[ 6.484488] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 6.490162] NET: Registered protocol family 17
[ 6.494688] NET: Registered protocol family 15
[ 6.499269] can: controller area network core (rev 20090105 abi 8)
[ 6.505580] NET: Registered protocol family 29
[ 6.510158] can: raw protocol (rev 20090105)
[ 6.514492] can: broadcast manager protocol (rev 20090105 t)
[ 6.520338] Bluetooth: RFCOMM TTY layer initialized
[ 6.525344] Bluetooth: RFCOMM socket layer initialized
[ 6.530707] Bluetooth: RFCOMM ver 1.11
[ 6.534573] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 6.539962] Bluetooth: BNEP filters: protocol multicast
[ 6.545304] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 6.551479] lib80211: common routines for IEEE802.11 drivers
[ 6.557257] lib80211_crypt: registered algorithm 'NULL'
[ 6.562560] lib80211_crypt: registered algorithm 'WEP'
[ 6.567816] lib80211_crypt: registered algorithm 'CCMP'
[ 6.573116] lib80211_crypt: registered algorithm 'TKIP'
[ 6.578415] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 6.586678] Bus freq driver module loaded
[ 6.590826] Bus freq driver Enabled
[ 6.597348] mxc_dvfs_core_probe
[ 6.600817] DVFS driver module loaded
[ 6.608061] regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
[ 6.622104] regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
[ 6.632470] regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on
[ 6.652153] regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on
[ 6.660328] snvs_rtc snvs_rtc.0: setting system clock to 2016-06-21 09:00:04 UTC (1466499604)
[ 6.673549] Freeing init memory: 248K
[ 13.651271] healthd: No charger supplies found
[ 13.655900] healthd: BatteryVoltagePath not found
[ 13.660358] init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
[ 13.664088] init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead
[ 13.664182] init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead
[ 13.664252] init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
[ 13.698478] healthd: BatteryTemperaturePath not found
[ 13.703631] binder: 2164:2164 transaction failed 29189, size 0-0
[ 13.811094] init: cannot find '/system/bin/ingsvcd', disabling 'ing'
[ 13.821221] init: property 'sys.powerctl' doesn't exist while expanding '${sys.powerctl}'
[ 13.829587] init: powerctl: cannot expand '${sys.powerctl}'
[ 13.835269] init: property 'sys.sysctl.extra_free_kbytes' doesn't exist while expanding '${sys.sysctl.extra_free_kbytes}'
[ 13.846367] init: cannot expand '${sys.sysctl.extra_free_kbytes}' while writing to '/proc/sys/vm/extra_free_kbytes'
[ 13.857294] android_usb: already disabled
[ 13.861761] mtp_bind_config
[ 13.864669] adb_bind_config
[ 13.870838] adb_open
[ 13.938269] SELinux: initialized (dev fuse, type fuse), uses genfs_contexts
root@tek_mx6:/ # [ 14.170613] EXT4-fs (mmcblk0p5): re-mounted. Opts: (null)
[ 14.784683] EXT4-fs (mmcblk0p5): re-mounted. Opts: (null)
[ 15.172715] imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00100000
[ 15.198549] imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
[ 16.523933] init: untracked pid 2511 exited
[ 17.737322] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
[ 18.006650] init: untracked pid 2520 exited
[ 21.693557] warning: `zygote' uses 32-bit capabilities (legacy support in use)
root@tek_mx6:/ #
root@tek_mx6:/ #
root@tek_mx6:/ #
root@tek_mx6:/ # [ 27.768080] request_suspend_state: wakeup (3->0) at 27529646670 (2016-06-21 09:00:25.598727003 UTC)
c[ 29.793595] Calling CRDA to update world regulatory domain
[ 29.799459] World regulatory domain updated:
[ 29.803849] (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
[ 29.811436] (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[ 29.818616] (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
[ 29.825783] (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
[ 29.832907] (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[ 29.840085] (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
d data[ 30.812317] <6>ath6kl: 3VAP/1, P2P enable, concurrent on , with dedicate p2p-device, multi-channel-concurrent enable, p2p-compat disable, sta-p2p-ie removed, p2p_wise_scan enable
[ 30.829846] <6>ath6kl: target bootstrap: 0x00000810
[ 30.854011] <6>ath6kl: target's subtype is 0x7, HT20/40 2SS Dual-band
[ 30.864863] <6>ath6kl: Create HTC cookie, type 1 num 440
[ 30.870637] <6>ath6kl: Create HTC cookie, type 2 num 66
[ 30.876015] <6>ath6kl: P2P flowctrl enabled
[ 30.876024] <6>ath6kl: RX aggregation drop disabled
[ 30.876031] <6>ath6kl: Using driver's regdb.
/[ 30.939982] acc_open
[ 30.942301] acc_release
[ 31.115052] <6>ath6kl: ar6004 hw 3.0 usb fw 5.0.0.79
[ 31.124788] <6>ath6kl: Wait defer tasks done...
58
61
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
67
67
66
66
66
66
67
66
66
65
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
66
67
66
66
66
66
67
66
67
67
67
66
66
66
66
66
~
root@tek_mx6:/data # busybox less /data/temperature.l[ 754.516956] init: untracked pid 3571 exited
130|root@tek_mx6:/data # ls
app
app-asec
app-lib
app-private
backup
bugreports
dalvik-cache
data
dontpanic
drm
local
log
lost+found
media
mediadrm
medusa
misc
property
resource-cache
security
ssh
system
temperature.log
temptest.sh
tombstones
user
root@tek_mx6:/data # [ 1208.158108] init: untracked pid 3862 exited
[ 1567.482610] SysRq : Emergency Remount R/O
[ 1567.497793] EXT4-fs (mmcblk0p4): re-mounted. Opts: (null)
[ 1567.590108] imx2-wdt imx2-wdt.0: Device shutdown: Expect reboot!
[ 1567.596288] Restarting system with command ''.
U-Boot 2009.08 (Jun 12 2016 - 10:45:30)
CPU: Freescale i.MX6 family TO1.5 at 792 MHz
Thermal sensor with ratio = 178
Temperature: 67 C, calibration data 0x5684d769
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63015 [WDOG ]
Boot Device: SD
I2C: ready
DRAM: 2 GB
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2
*** Warning - bad CRC or MMC, using default environment
In: serial
Out: serial
Err: serial
Found PFUZE100! deviceid=10,revid=21
Net: No ethernet found.
hw version:1
Hit any key to stop autoboot: 0
kernel @ 10808000 (4734496)
ramdisk @ 11800000 (1838792)
kernel cmdline:
use boot.img command line:
console=ttymxc1,115200 init=/init video=mxcfb0:dev=ldb,LDB-WSVGA,if=RGB24,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc1 androidboot.hardware=freescale maxcpus=4 no_console_suspend=1 androidboot.serialno=121a11d4e315dec4 hw_rev=1
Starting kernel ...
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Linux version 3.0.35-00003-g041d520 (kris@ecovacs) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #284 SMP PREEMPT Tue Jun 21 11:11:58 CST 2016
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board
[ 0.000000] Ignoring unrecognised tag 0x54410008
[ 0.000000] hw_rev:1
[ 0.000000] Memory policy: ECC disabled, Data cache writealloc
[ 0.000000] CPU identified as i.MX6Q, unknown revision
[ 0.000000] PERCPU: Embedded 7 pages/cpu @c29ce000 s6528 r8192 d13952 u32768
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 468224
[ 0.000000] Kernel command line: console=ttymxc1,115200 init=/init video=mxcfb0:dev=ldb,LDB-WSVGA,if=RGB24,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc1 androidboot.hardware=freescale maxcpus=4 no_console_suspend=1 androidboot.serialno=121a11d4e315dec4 hw_rev=1
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 379MB 378MB 848MB 240MB = 1845MB total
[ 0.000000] Memory: 1859580k/1859580k available, 237572k reserved, 1489920K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xfbe00000 - 0xffe00000 ( 64 MB)
[ 0.000000] vmalloc : 0xd9800000 - 0xf2000000 ( 392 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd9000000 ( 400 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .init : 0xc0008000 - 0xc0046000 ( 248 kB)
[ 0.000000] .text : 0xc0046000 - 0xc08aa534 (8594 kB)
[ 0.000000] .data : 0xc08ac000 - 0xc0927258 ( 493 kB)
[ 0.000000] .bss : 0xc092727c - 0xc0aaf5bc (1569 kB)
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] NR_IRQS:624
[ 0.000000] MXC GPIO hardware
[ 0.000000] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
[ 0.000000] arm_max_freq=1GHz
[ 0.000000] MXC_Early serial console at MMIO 0x21e8000 (options '115200')
[ 0.000000] bootconsole [ttymxc1] enabled
[ 0.235642] Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
[ 0.328376] pid_max: default: 32768 minimum: 301
[ 0.333164] Security Framework initialized
[ 0.337321] SELinux: Initializing.
[ 0.340965] Mount-cache hash table entries: 512
[ 0.346268] Initializing cgroup subsys debug
[ 0.350595] Initializing cgroup subsys cpuacct
[ 0.355102] Initializing cgroup subsys freezer
[ 0.359593] CPU: Testing write buffer coherency: ok
[ 0.364802] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
[ 0.485457] CPU1: Booted secondary processor
[ 0.635477] CPU2: Booted secondary processor
[ 0.735446] CPU3: Booted secondary processor
[ 0.794797] Brought up 4 CPUs
[ 0.810625] SMP: Total of 4 processors activated (6324.22 BogoMIPS).
[ 0.840599] print_constraints: dummy:
[ 0.844622] NET: Registered protocol family 16
[ 0.854485] print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal
[ 0.862045] print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal
[ 0.869882] print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal
[ 0.877613] print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal
[ 0.885427] print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal
[ 0.893154] print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal
[ 0.903724] ram_console: got buffer at 3ff00000, size 100000
[ 0.909533] ram_console: found existing buffer, size 35242, start 35242
[ 1.003123] console [ram-1] enabled
[ 1.171072] hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
[ 1.177993] hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
[ 1.185495] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 1.191459] L310 cache controller enabled
[ 1.195641] l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B
[ 1.239330] bio: create slab <bio-0> at 0
[ 1.247360] mxs-dma mxs-dma-apbh: initialized
[ 1.252191] print_constraints: vmmc: 3300 mV
[ 1.257612] vgaarb: loaded
[ 1.261626] SCSI subsystem initialized
[ 1.266403] usbcore: registered new interface driver usbfs
[ 1.272206] usbcore: registered new interface driver hub
[ 1.277856] usbcore: registered new device driver usb
[ 1.283078] Freescale USB OTG Driver loaded, $Revision: 1.55 $
[ 1.295784] mc_pfuze 1-0008: ID: 0,Full lay: 2 ,Metal lay: 1
[ 1.303820] mc_pfuze 1-0008: FAB: 0 ,FIN: 0
[ 1.324112] pfuze100_init:Revision ID:21,arm_max_freq=2,enable_ldo_mode=1
[ 1.360796] pfuze100 init: set SWBST-----------==========>
[ 1.372608] print_constraints: PFUZE100_SW1A: 300 <--> 1875 mV at 1300 mV
[ 1.382114] print_constraints: PFUZE100_SW1B: 300 <--> 1875 mV at 300 mV
[ 1.395276] print_constraints: PFUZE100_SW1C: 300 <--> 1875 mV at 1300 mV
[ 1.404779] print_constraints: PFUZE100_SW2: 800 <--> 3950 mV at 3300 mV
[ 1.414115] print_constraints: PFUZE100_SW3A: 400 <--> 1975 mV at 1500 mV
[ 1.423610] print_constraints: PFUZE100_SW3B: 400 <--> 1975 mV at 1500 mV
[ 1.433117] print_constraints: PFUZE100_SW4: 800 <--> 3950 mV at 3150 mV
[ 1.442459] print_constraints: PFUZE100_SWBST: 5000 <--> 5150 mV at 5000 mV
[ 1.452124] print_constraints: PFUZE100_VSNVS: 1200 <--> 3000 mV at 1800 mV
[ 1.463332] print_constraints: PFUZE100_VREFDDR: at 750 mV
[ 1.471510] print_constraints: PFUZE100_VGEN1: 800 <--> 1550 mV at 1500 mV
[ 1.481081] print_constraints: PFUZE100_VGEN2: 800 <--> 1550 mV at 1500 mV
[ 1.490614] print_constraints: PFUZE100_VGEN3: 1800 <--> 3300 mV at 2800 mV
[ 1.504096] print_constraints: PFUZE100_VGEN4: 1800 <--> 3300 mV at 1800 mV
[ 1.517521] print_constraints: PFUZE100_VGEN5: 1800 <--> 3300 mV at 3000 mV
[ 1.527182] print_constraints: PFUZE100_VGEN6: 1800 <--> 3300 mV at 3300 mV
[ 1.554880] imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 1.562925] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 1.570464] Bluetooth: Core ver 2.16
[ 1.574290] NET: Registered protocol family 31
[ 1.578905] Bluetooth: HCI device and connection manager initialized
[ 1.585369] Bluetooth: HCI socket layer initialized
[ 1.590405] Bluetooth: L2CAP socket layer initialized
[ 1.595580] Bluetooth: SCO socket layer initialized
[ 1.601070] i2c-core: driver [max17135] using legacy suspend method
[ 1.607452] i2c-core: driver [max17135] using legacy resume method
[ 1.613819] Switching to clocksource mxc_timer1
[ 1.631549] NET: Registered protocol family 2
[ 1.636179] IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 1.643897] TCP established hash table entries: 65536 (order: 7, 524288 bytes)
[ 1.652304] TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
[ 1.660140] TCP: Hash tables configured (established 65536 bind 65536)
[ 1.666826] TCP reno registered
[ 1.670075] UDP hash table entries: 256 (order: 1, 8192 bytes)
[ 1.676079] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
[ 1.682858] NET: Registered protocol family 1
[ 1.687755] RPC: Registered named UNIX socket transport module.
[ 1.693799] RPC: Registered udp transport module.
[ 1.698618] RPC: Registered tcp transport module.
[ 1.703474] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.710025] PCI: CLS 0 bytes, default 32
[ 1.714285] Unpacking initramfs...
[ 1.837428] Freeing initrd memory: 1792K
[ 1.842546] PMU: registered new PMU device of type 0
[ 1.847808] Static Power Management for Freescale i.MX6
[ 1.853151] wait mode is enabled for i.MX6
[ 1.857598] cpaddr = d9880000 suspend_iram_base=d98fc000
[ 1.863108] PM driver module loaded
[ 1.867113] IMX usb wakeup probe
[ 1.870611] the wakeup pdata is 0xd43296e0
[ 1.875188] add wake up source irq 75
[ 1.885624] IMX usb wakeup probe
[ 1.889122] the wakeup pdata is 0xd43294a0
[ 1.893852] cpu regulator mode:ldo_bypass
[ 1.906198] _regulator_get: get() with no identifier
[ 1.911337] mx6_cpu_regulator_init: failed to get pu regulator
[ 1.925675] i.MXC CPU frequency driver
[ 1.930169] audit: initializing netlink socket (disabled)
[ 1.935676] type=2000 audit(1.690:1): initialized
[ 1.961784] highmem bounce pool size: 64 pages
[ 1.966566] ashmem: initialized
[ 1.970968] NTFS driver 2.1.30 [Flags: R/O].
[ 1.975480] JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 1.981844] fuse init (API version 7.16)
[ 1.986122] msgmni has been set to 725
[ 1.989985] SELinux: Registering netfilter hooks
[ 1.996260] NET: Registered protocol family 38
[ 2.001046] cryptodev: driver loaded.
[ 2.004802] io scheduler noop registered
[ 2.008817] io scheduler deadline registered
[ 2.013270] io scheduler cfq registered (default)
[ 2.019461] MIPI DSI driver module loaded
[ 2.023739] mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb
[ 2.030263] _regulator_get: get() with no identifier
[ 2.037409] mxc_sdc_fb mxc_sdc_fb.1: Can't get fb option for mxcfb1!
[ 2.043947] mxc_sdc_fb mxc_sdc_fb.2: Can't get fb option for mxcfb2!
[ 2.050472] mxc_sdc_fb mxc_sdc_fb.3: Can't get fb option for mxcfb3!
[ 2.056912] imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00100000
[ 2.064777] imx-sdma imx-sdma: loaded firmware 1.1
[ 2.074760] imx-sdma imx-sdma: initialized
[ 2.205963] Serial: IMX driver
[ 2.209237] imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
[ 2.216150] imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX
[ 2.222767] console [ttymxc1] enabled, bootconsole disabled
[ 2.222767] console [ttymxc1] enabled, bootconsole disabled
[ 2.234439] imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
[ 2.241429] imx-uart.3: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX
[ 2.254664] loop: module loaded
[ 2.257936] at24 2-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write
[ 2.265180] xmf10411_i2c_probe
[ 2.268518] ks103_us_probe
[ 2.271293] ks103-ultrasonic 1-0073: I2C Address: 0x73
[ 2.277161] ks103-ultrasonic 1-0073: Write to device fails status fffffffb
[ 2.284172] ks103-ultrasonic 1-0073: Read year failed. ret:-5
[ 2.290050] ks103-ultrasonic 1-0073: Read version failed:-5
[ 2.295694] ks103-ultrasonic: probe of 1-0073 failed with error -5
[ 2.302014] ks103_us_probe
[ 2.304785] ks103-ultrasonic 1-0074: I2C Address: 0x74
[ 2.310652] ks103-ultrasonic 1-0074: Write to device fails status fffffffb
[ 2.317647] ks103-ultrasonic 1-0074: Read year failed. ret:-5
[ 2.323473] ks103-ultrasonic 1-0074: Read version failed:-5
[ 2.329183] ks103-ultrasonic: probe of 1-0074 failed with error -5
[ 2.335439] ks103_us_probe
[ 2.338263] ks103-ultrasonic 1-0075: I2C Address: 0x75
[ 2.344132] ks103-ultrasonic 1-0075: Write to device fails status fffffffb
[ 2.351139] ks103-ultrasonic 1-0075: Read year failed. ret:-5
[ 2.356950] ks103-ultrasonic 1-0075: Read version failed:-5
[ 2.362656] ks103-ultrasonic: probe of 1-0075 failed with error -5
[ 2.370717] GPMI NAND driver registered. (IMX)
[ 2.376250] vcan: Virtual CAN interface driver
[ 2.380779] CAN device driver interface
[ 2.384680] flexcan netdevice driver
[ 2.388566] FEC Ethernet Driver
[ 2.391926] PPP generic driver version 2.4.2
[ 2.396628] PPP Deflate Compression module registered
[ 2.401817] PPP BSD Compression module registered
[ 2.407084] PPP MPPE Compression module registered
[ 2.412021] NET: Registered protocol family 24
[ 2.416550] tun: Universal TUN/TAP device driver, 1.6
[ 2.421680] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
[ 2.428598] usbcore: registered new interface driver asix
[ 2.434192] usbcore: registered new interface driver cdc_ether
[ 2.440295] usbcore: registered new interface driver cdc_eem
[ 2.446149] usbcore: registered new interface driver dm9601
[ 2.451983] usbcore: registered new interface driver net1080
[ 2.457839] usbcore: registered new interface driver cdc_subset
[ 2.464029] usbcore: registered new interface driver zaurus
[ 2.469695] cdc_ncm: 04-Aug-2011
[ 2.473122] usbcore: registered new interface driver cdc_ncm
[ 2.478873] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.485689] fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
[ 2.492408] fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
[ 2.528522] fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
[ 2.548513] fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
[ 2.554802] hub 1-0:1.0: USB hub found
[ 2.558648] hub 1-0:1.0: 1 port detected
[ 2.562888] add wake up source irq 72
[ 2.566655] fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
[ 2.573419] fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
[ 2.608523] fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200
[ 2.628510] fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
[ 2.634789] hub 2-0:1.0: USB hub found
[ 2.638685] hub 2-0:1.0: 1 port detected
[ 2.643083] Initializing USB Mass Storage driver...
[ 2.648198] usbcore: registered new interface driver usb-storage
[ 2.654342] USB Mass Storage support registered.
[ 2.659036] ARC USBOTG Device Controller driver (1 August 2005)
[ 2.668372] android_usb gadget: Mass Storage Function, version: 2009/09/11
[ 2.675338] android_usb gadget: Number of LUNs=1
[ 2.680088] lun0: LUN: removable file: (no medium)
[ 2.685564] Gadget Android: controller 'fsl-usb2-udc' not recognized
[ 2.692063] android_usb gadget: android_usb ready
[ 2.696831] Suspend udc for OTG auto detect
[ 2.701155] USB Host suspend begins
[ 2.704706] will suspend roothub and its children
[ 2.709500] ehci_fsl_bus_suspend begins, DR
[ 2.713817] ehci_fsl_bus_suspend ends, DR
[ 2.717896] host suspend ends
[ 2.720942] USB Gadget resume begins
[ 2.724636] fsl_udc_resume, Wait for wakeup thread finishes
[ 2.733501] dr_controller_run: udc enter low power mode
[ 2.738944] USB Gadget resume ends
[ 2.742410] fsl-usb2-udc: bind to driver android_usb
[ 2.747971] mousedev: PS/2 mouse device common for all mice
[ 2.754190] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[ 2.783213] gt911-touch 2-0014: i2c test failed attempt 1: -5
[ 2.809164] gt911-touch 2-0014: i2c test failed attempt 2: -5
[ 2.838528] gt911-touch 2-0014: I2C communication failure: -5
[ 2.844400] gt911-touch: probe of 2-0014 failed with error -5
[ 2.907579] ft5x06-touch 2-0038: IC Version:0xa6
[ 2.912560] input: FocalTech Capacitive TouchScreen as /devices/virtual/input/input1
[ 2.921420] i2c-core: driver [isl29023] using legacy suspend method
[ 2.927754] i2c-core: driver [isl29023] using legacy resume method
[ 2.935299] using rtc device, snvs_rtc, for alarms
[ 2.940028] snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
[ 2.947076] i2c /dev entries driver
[ 2.951469] Linux video capture interface: v2.00
[ 2.958559] usb 2-1: new high speed USB device number 2 using fsl-ehci
[ 3.110055] hub 2-1:1.0: USB hub found
[ 3.113965] hub 2-1:1.0: 4 ports detected
[ 3.398609] usb 2-1.1: new high speed USB device number 3 using fsl-ehci
[ 3.478716] USB Gadget resume begins
[ 3.482412] fsl_udc_resume, Wait for wakeup thread finishes
[ 3.658608] usb 2-1.2: new high speed USB device number 4 using fsl-ehci
[ 6.003533] ov10635_set_regs ok
[ 6.012235] ov10635 0-0030: ov10635 Product ID a6 Manufacturer ID 35
[ 6.018676] ov10635 probe end
[ 6.022362] mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
[ 6.030086] mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
[ 6.037826] uvcvideo: Found UVC 1.00 device USB 2.0 Camera (0c45:62f1)
[ 6.049687] input: USB 2.0 Camera as /devices/platform/fsl-ehci.1/usb2/2-1/2-1.1/2-1.1:1.0/input/input2
[ 6.059570] usbcore: registered new interface driver uvcvideo
[ 6.065434] USB Video Class driver (v1.1.0)
[ 6.070287] i2c-core: driver [mag3110] using legacy suspend method
[ 6.076587] i2c-core: driver [mag3110] using legacy resume method
[ 6.083248] imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
[ 6.091659] device-mapper: uevent: version 1.0.3
[ 6.096679] device-mapper: ioctl: 4.20.0-ioctl (2011-02-02) initialised: dm-devel@redhat.com
[ 6.105234] Bluetooth: Virtual HCI driver ver 1.3
[ 6.110293] Bluetooth: HCI UART driver ver 2.2
[ 6.114803] Bluetooth: HCIATH3K protocol initialized
[ 6.119848] Bluetooth: Generic Bluetooth USB driver ver 0.6
[ 6.125654] usbcore: registered new interface driver btusb
[ 6.131613] sdhci: Secure Digital Host Controller Interface driver
[ 6.137913] sdhci: Copyright(c) Pierre Ossman
[ 6.142442] sdhci sdhci-esdhc-imx.2: no card-detect pin available!
[ 6.149041] mmc0: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA
[ 6.156250] sdhci sdhci-esdhc-imx.3: no write-protect pin available!
[ 6.166021] mmc1: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA
[ 6.173258] sdhci sdhci-esdhc-imx.1: no write-protect pin available!
[ 6.179694] sdhci sdhci-esdhc-imx.1: no card-detect pin available!
[ 6.189254] mmc2: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA
[ 6.198640] mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[ 6.211752] VPU initialized
[ 6.215628] mxc_asrc registered
[ 6.219140] Galcore version 4.6.9.9754
[ 6.254456] Thermal calibration data is 0x5684d769
[ 6.259333] Thermal sensor with ratio = 178
[ 6.278507] Anatop Thermal registered as thermal_zone0
[ 6.283894] anatop_thermal_probe: default cooling device is cpufreq!
[ 6.291953] usbcore: registered new interface driver usbhid
[ 6.297593] usbhid: USB HID core driver
[ 6.302143] logger: created 256K log 'log_main'
[ 6.306978] logger: created 256K log 'log_events'
[ 6.311993] logger: created 256K log 'log_radio'
[ 6.316958] logger: created 256K log 'log_system'
[ 6.351624] mmc0: new high speed SDHC card at address aaaa
[ 6.357703] mmcblk0: mmc0:aaaa SS08G 7.40 GiB
[ 6.367359] mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
[ 6.372640] mmcblk0: p4 size 13352010 extends beyond EOD, truncated
[ 6.478747] AIC3254: programming mini dsp
[ 6.482827] The register sections found in pps header file:
[ 6.488531] miniDSP_A_reg_values
[ 6.491820] miniDSP_D_reg_values
[ 6.495168] Registered minidsp driver, Major number: 247
[ 6.503150] asoc: tlv320aic32x4-hifi <-> imx-ssi.1 mapping ok
[ 6.509977] ALSA device list:
[ 6.513012] #0: aic3254-audio
[ 6.516636] oprofile: using arm/armv7-ca9
[ 6.523247] u32 classifier
[ 6.526071] Actions configured
[ 6.529554] Netfilter messages via NETLINK v0.30.
[ 6.534367] nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
[ 6.544747] ctnetlink v0.93: registering with nfnetlink.
[ 6.550173] NF_TPROXY: Transparent proxy support initialized, version 4.1.0
[ 6.557251] NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
[ 6.563587] xt_time: kernel timezone is -0000
[ 6.568184] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 6.573743] arp_tables: (C) 2002 David S. Miller
[ 6.578535] TCP cubic registered
[ 6.581827] Initializing XFRM netlink socket
[ 6.586352] NET: Registered protocol family 10
[ 6.598286] Mobile IPv6
[ 6.600851] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 6.606452] NET: Registered protocol family 17
[ 6.611050] NET: Registered protocol family 15
[ 6.615558] can: controller area network core (rev 20090105 abi 8)
[ 6.621933] NET: Registered protocol family 29
[ 6.626448] can: raw protocol (rev 20090105)
[ 6.630850] can: broadcast manager protocol (rev 20090105 t)
[ 6.636689] Bluetooth: RFCOMM TTY layer initialized
[ 6.641664] Bluetooth: RFCOMM socket layer initialized
[ 6.646918] Bluetooth: RFCOMM ver 1.11
[ 6.650874] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 6.656302] Bluetooth: BNEP filters: protocol multicast
[ 6.661605] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 6.667827] lib80211: common routines for IEEE802.11 drivers
[ 6.673569] lib80211_crypt: registered algorithm 'NULL'
[ 6.678926] lib80211_crypt: registered algorithm 'WEP'
[ 6.684128] lib80211_crypt: registered algorithm 'CCMP'
[ 6.689482] lib80211_crypt: registered algorithm 'TKIP'
[ 6.694816] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 6.703085] Bus freq driver module loaded
[ 6.707169] Bus freq driver Enabled
[ 6.713692] mxc_dvfs_core_probe
[ 6.717182] DVFS driver module loaded
[ 6.724440] regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
[ 6.734803] regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
[ 6.745082] regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on
[ 6.759129] regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on
[ 6.767350] snvs_rtc snvs_rtc.0: setting system clock to 2016-06-21 09:26:20 UTC (1466501180)
[ 6.780608] Freeing init memory: 248K
[ 10.948796] healthd: No charger supplies found
[ 10.953361] healthd: BatteryVoltagePath not found
[ 10.958028] init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
[ 10.966656] healthd: BatteryTemperaturePath not found
[ 10.971905] binder: 2164:2164 transaction failed 29189, size 0-0
[ 11.014315] init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead
[ 11.023698] init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead
[ 11.034076] init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
root@tek_mx6:/ # [ 11.220891] init: cannot find '/system/bin/ingsvcd', disabling 'ing'
[ 11.230980] init: property 'sys.powerctl' doesn't exist while expanding '${sys.powerctl}'
[ 11.239320] init: powerctl: cannot expand '${sys.powerctl}'
[ 11.244995] init: property 'sys.sysctl.extra_free_kbytes' doesn't exist while expanding '${sys.sysctl.extra_free_kbytes}'
[ 11.256356] init: cannot expand '${sys.sysctl.extra_free_kbytes}' while writing to '/proc/sys/vm/extra_free_kbytes'
[ 11.267170] android_usb: already disabled
[ 11.271524] mtp_bind_config
[ 11.274411] adb_bind_config
[ 11.280242] adb_open
[ 11.290408] SELinux: initialized (dev fuse, type fuse), uses genfs_contexts
[ 11.322882] EXT4-fs (mmcblk0p5): re-mounted. Opts: (null)
[ 11.952260] EXT4-fs (mmcblk0p5): re-mounted. Opts: (null)
[ 12.170062] imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00100000
[ 12.188623] imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
[ 13.162894] init: untracked pid 2431 exited
[ 14.048501] ov10635_write_reg:write reg error:reg=300c,val=61
[ 14.618493] ov10635_write_reg:write reg error:reg=103,val=1
[ 14.908379] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
[ 15.523163] init: untracked pid 2526 exited
[ 16.972568] warning: `zygote' uses 32-bit capabilities (legacy support in use)
[ 24.266858] request_suspend_state: wakeup (3->0) at 24028372671 (2016-06-21 09:26:37.988767670 UTC)
[ 27.907994] Calling CRDA to update world regulatory domain
[ 27.916662] World regulatory domain updated:
[ 27.921057] (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
[ 27.928697] (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[ 27.935823] (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
[ 27.943001] (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm)
[ 27.950182] (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[ 27.960019] (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm)
[ 28.142113] acc_open
[ 28.144433] acc_release
[ 28.353847] <6>ath6kl: 3VAP/1, P2P enable, concurrent on , with dedicate p2p-device, multi-channel-concurrent enable, p2p-compat disable, sta-p2p-ie removed, p2p_wise_scan enable
[ 28.371333] <6>ath6kl: target bootstrap: 0x00000810
[ 29.295727] <6>ath6kl: target's subtype is 0x7, HT20/40 2SS Dual-band
[ 29.306188] <6>ath6kl: Create HTC cookie, type 1 num 440
[ 29.311672] <6>ath6kl: Create HTC cookie, type 2 num 66
[ 29.317585] <6>ath6kl: P2P flowctrl enabled
[ 29.322176] <6>ath6kl: RX aggregation drop disabled
[ 29.327161] <6>ath6kl: Using driver's regdb.
[ 29.608517] <6>ath6kl: ar6004 hw 3.0 usb fw 5.0.0.79
[ 29.614689] <6>ath6kl: Wait defer tasks done...
[ 30.032520] <6>ath6kl: Create dedicated p2p interface
[ 30.048573] Calling CRDA for country: 6A
[ 30.290430] <6>ath6kl: Enable Firmware crash notiry.
[ 30.307638] usbcore: registered new interface driver ath6kl_usb
[ 30.374284] ehci_fsl_bus_resume begins, DR
[ 30.973004] ADDRCONF(NETDEV_UP): wlan0: link is not ready
[ 31.998314] ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready
[ 32.770727] qtaguid: iface_stat: stat_update() wlan0 not found
[ 34.130183] type=1400 audit(1466501207.850:5): avc: denied { getattr } for pid=2795 comm="zygote" path="socket:[3577]" dev=sockfs ino=3577 scontext=u:r:untrusted_app:s0 tcontext=u:r:zygote:s0 tclass=unix_stream_socket
[ 34.155525] type=1400 audit(1466501207.870:6): avc: denied { getopt } for pid=2795 comm="zygote" path="/dev/socket/zygote" scontext=u:r:untrusted_app:s0 tcontext=u:r:zygote:s0 tclass=unix_stream_socket
[ 34.536580] type=1400 audit(1466501208.250:7): avc: denied { getattr } for pid=2795 comm="ebot.serviceapp" path="/data/app" dev=mmcblk0p4 ino=348817 scontext=u:r:untrusted_app:s0 tcontext=u:object_r:apk_data_file:s0 tclass=dir
[ 34.865913] type=1400 audit(1466501208.580:8): avc: denied { write } for pid=2795 comm="ebot.serviceapp" name="/" dev=tmpfs ino=3193 scontext=u:r:untrusted_app:s0 tcontext=u:object_r:tmpfs:s0 tclass=dir
[ 34.884683] type=1400 audit(1466501208.600:9): avc: denied { add_name } for pid=2795 comm="ebot.serviceapp" name="tts.pcm" scontext=u:r:untrusted_app:s0 tcontext=u:object_r:tmpfs:s0 tclass=dir
[ 34.902620] type=1400 audit(1466501208.620:10): avc: denied { create } for pid=2795 comm="ebot.serviceapp" name="tts.pcm" scontext=u:r:untrusted_app:s0 tcontext=u:object_r:untrusted_app_tmpfs:s0 tclass=file
[ 34.922092] type=1400 audit(1466501208.640:11): avc: denied { write open } for pid=2795 comm="ebot.serviceapp" name="tts.pcm" dev=tmpfs ino=3790 scontext=u:r:untrusted_app:s0 tcontext=u:object_r:untrusted_app_tmpfs:s0 tclass=file
[ 34.943760] type=1400 audit(1466501208.660:12): avc: denied { getattr } for pid=2795 comm="ebot.serviceapp" path="/tmp/tts.pcm" dev=tmpfs ino=3790 scontext=u:r:untrusted_app:s0 tcontext=u:object_r:untrusted_app_tmpfs:s0 tclass=file
[ 34.988017] type=1400 audit(1466501208.700:13): avc: denied { setattr } for pid=2837 comm="chmod" name="tts.pcm" dev=tmpfs ino=3790 scontext=u:r:untrusted_app:s0 tcontext=u:object_r:untrusted_app_tmpfs:s0 tclass=file
[ 35.071232] cpufreq_interactive_input_connect: connect to FocalTech Capacitive TouchScreen
[ 35.742768] init: sys_prop: permission denied uid:1003 name:service.bootanim.exit
[ 37.774228] type=1400 audit(1466501211.490:14): avc: denied { read } for pid=2875 comm="Thread-45" name="ttymxc0" dev=tmpfs ino=5125 scontext=u:r:untrusted_app:s0 tcontext=u:object_r:device:s0 tclass=chr_file
[ 45.388511] wlan0: no IPv6 routers present
[ 46.998528] VPU blocking: timeout.
[ 47.528544] VPU blocking: timeout.
[ 48.028508] VPU blocking: timeout.
[ 48.978520] VPU blocking: timeout.
[ 49.478522] VPU blocking: timeout.
[ 49.978520] VPU blocking: timeout.
[ 50.488518] VPU blocking: timeout.
[ 50.988511] VPU blocking: timeout.
[ 51.488506] VPU blocking: timeout.
[ 51.988513] VPU blocking: timeout.
[ 52.968497] VPU blocking: timeout.
[ 53.478512] VPU blocking: timeout.
[ 54.248540] ov10635_write_reg:write reg error:reg=103,val=1
[ 54.740596] VPU blocking: timeout.
[ 55.238524] VPU blocking: timeout.
[ 55.738567] VPU blocking: timeout.
[ 56.238512] VPU blocking: timeout.
[ 56.958509] VPU blocking: timeout.
[ 57.478649] VPU blocking: timeout.
[ 58.328522] ov10635_write_reg:write reg error:reg=3621,val=64
[ 58.334474] mxc_v4l2_s_param: vidioc_int_s_parm returned an error -1
[ 59.939165] audit_printk_skb: 12 callbacks suppressed
[ 59.944502] type=1400 audit(1466501233.660:19): avc: denied { write } for pid=2917 comm="Thread-45" scontext=u:r:untrusted_app:s0 tcontext=u:r:untrusted_app:s0 tclass=netlink_route_socket
[ 64.998502] VPU blocking: timeout.
[ 72.088506] VPU blocking: timeout.
root@tek_mx6:/ #
root@tek_mx6:/ #
[ 97.460862] init: untracked pid 2978 exited
root@tek_mx6:/ #
If the bitrate is set (CBR), perhaps the resolution vs. bitrate relation is causing the VPU to block sometimes (when not getting enough information to process a frame).
The VPU blocking timeout is safe to be ingnored if this does not have a big impact on video performance,
it's normal that VPU can block some times but it must not affect your performance.
Please try setting the bitrate a bit greater (if possible).
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------