"AVC reordering" issue when availing hardware codec on i.MX8 QuadXPlus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"AVC reordering" issue when availing hardware codec on i.MX8 QuadXPlus

1,502 Views
schinda1
Contributor II

Hello,

We are facing below errors when availing hardware codec for increased performance. We are currently using this sample Native Codec OpenGL based application as litmus test :  https://github.com/android/ndk-samples/tree/master/native-codec

com.example.nativecodec I/ACodec: Send reorder config(0) to VPU

com.example.nativecodec E/ACodec: disable AVC reorder failed

com.example.nativecodec E/ACodec: [OMX.Freescale.std.video_decoder.avc.v3.hw-based] setPortMode on output to DynamicANWBuffer failed w/ err -1010

Can you please assist ?

[UPDATE] : Related "Speculative" CMA  question : https://community.nxp.com/thread/523757

Tags (1)
0 Kudos
Reply
1 Reply

1,385 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Sharat,

Whether the issue can be reproduced in i.MX8QXP MEK board? 

Except such errors, is there other side effect?

Regards

0 Kudos
Reply