question with u-boot and linux kernel on SabreSD Platform

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

question with u-boot and linux kernel on SabreSD Platform

1,629 次查看
jingyizhang
Contributor I

followed these two documents to set up u-boot and linux

Linux on the i.MX6 sabre sd platform in a few commands

u-boot on the i.MX6 sabre sd platform in a few commands

versions installed:

u-boot version: v2015.07

linux kernel version: v3.14.28

when i try to boot, this is the serial output:

U-Boot 2015.07 (Jul 23 2015 - 17:42:18 -0400)

CPU:   Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)

CPU:   Automotive temperature grade (-40C to 125C) at 44C

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

PMIC:  PFUZE100 ID=0x10

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

PCI:   pcie phy link never came up

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

Net:   FEC [PRIME]

Hit any key to stop autoboot:  0

switch to partitions #0, OK

mmc1 is current device

reading boot.scr

** Unable to read file boot.scr **

reading zImage

** Unable to read file zImage **

Booting from net ...

FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !

BOOTP broadcast 1

BOOTP broadcast 2

BOOTP broadcast 3

BOOTP broadcast 4

BOOTP broadcast 5

....

can someone point out what's wrong with my setup?

标签 (3)
0 项奖励
回复
1 回复

1,439 次查看
Yuri
NXP Employee
NXP Employee

  Please stop U-boot and configure U-boot environment for Your boot device
as described in "i.MX_Linux_User's_Guide.pdf" in the FSL Linux documentation.

https://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&location=null&fasp=1&Par...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复