question about interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

question about interrupt

2,061 次查看
caibai
Contributor III

i use imx6sx-sd board and have some  question about how interrupt work

if i set GPIO6_2 as interrupt pin at both Cortex-A9 and Cortex-M4,when this pin is trigger,which core will handle this interrupt signal

i read <Getting_Started_with_Multicore_Programming_for_i.MX_6SoloX_V0.pdf> about low power function,it means that when Cortex-M4 set into low power mode , linux will close Cortex-M4 clock and  Cortex-M4 can't wake up by  interrupt direct. it only let linux register wake up interrupt souce and first wake up linux ,then linux open Cortex-M4 clock and let it run out low power mode ?

标签 (1)
0 项奖励
回复
3 回复数

1,862 次查看
igorpadykov
NXP Employee
NXP Employee

Hi cai

seems you are right: please check Table 10-1. Power Modes

i.MX6SX Reference Manual, its shows M4 as Always Clock Gated

in Stop mode.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,862 次查看
caibai
Contributor III

thank you for reply.

how CPU deal  with GPIO interrupt when Cortex-A9 and Cortex-M4 both configure it as interrupt

0 项奖励
回复

1,862 次查看
igorpadykov
NXP Employee
NXP Employee

please check Chapter 52 Resource Domain Controller (RDC)

0 项奖励
回复