qmlscene and qmlviewer are missing from fsl-image-qt5-validation-imx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

qmlscene and qmlviewer are missing from fsl-image-qt5-validation-imx

跳至解决方案
2,421 次查看
grigoritimonen
Contributor II

Hi,

We use a NXP IMX 8MM EVK with Yocto Linux 4.14.98_2.0.0 from NXP.

I made a fsl-image-qt5-validation-imx image and can run some QT examples on target device.

However, I can't see qmlviewer or qmlscene tools for UI prototyping.

I was trying to search for *scene* and *viewer* files under meta-qt5 directory and didn't find anything related.

Any clues on how to build qmlscene and install it?

标记 (3)
0 项奖励
回复
1 解答
2,249 次查看
grigoritimonen
Contributor II

Ok, I found that qmlscene is part of the SDK. So I was able to build a meta-toolchain-qt5 and copy /usr/bin/qt5/* to my rootfs.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,250 次查看
grigoritimonen
Contributor II

Ok, I found that qmlscene is part of the SDK. So I was able to build a meta-toolchain-qt5 and copy /usr/bin/qt5/* to my rootfs.

0 项奖励
回复