qmlscene and qmlviewer are missing from fsl-image-qt5-validation-imx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

qmlscene and qmlviewer are missing from fsl-image-qt5-validation-imx

Jump to solution
2,408 Views
grigoritimonen
Contributor II

Hi,

We use a NXP IMX 8MM EVK with Yocto Linux 4.14.98_2.0.0 from NXP.

I made a fsl-image-qt5-validation-imx image and can run some QT examples on target device.

However, I can't see qmlviewer or qmlscene tools for UI prototyping.

I was trying to search for *scene* and *viewer* files under meta-qt5 directory and didn't find anything related.

Any clues on how to build qmlscene and install it?

Tags (3)
0 Kudos
Reply
1 Solution
2,236 Views
grigoritimonen
Contributor II

Ok, I found that qmlscene is part of the SDK. So I was able to build a meta-toolchain-qt5 and copy /usr/bin/qt5/* to my rootfs.

View solution in original post

0 Kudos
Reply
1 Reply
2,237 Views
grigoritimonen
Contributor II

Ok, I found that qmlscene is part of the SDK. So I was able to build a meta-toolchain-qt5 and copy /usr/bin/qt5/* to my rootfs.

0 Kudos
Reply