pwm2 node(dts)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pwm2 node(dts)

919 Views
gtulsira
Contributor I
I tried this method and it didn't work, But /sys/class/pwm is empty.
 
please check and let me know the modification need to do for getting pwm2.
 

My modification is as follows:

imx8qxp.dtsi:

+       pwm2: pwm@5d020000 {
+               compatible = "fsl,imx8qxp-pwm", "fsl,imx27-pwm";
+               reg = <0x0 0x5d020000 0 0x10000>;
+               clock-names = "ipg", "per";
+               clocks = <&pwm2_lpcg 4>,
+               <&pwm2_lpcg 1>;
+               assigned-clocks = <&clk IMX_SC_R_PWM_2 IMX_SC_PM_CLK_PER>;
+               assigned-clock-rates = <24000000>;
+               power-domains = <&pd IMX_SC_R_PWM_2>;          
+               #pwm-cells = <2>;
+               status = "disabled";
+       };      
+
Add the following content to the DTS file of our board
inside &iomuxc {
pinctrl_pwm2_d: pwm2d {
                fsl,pins = <IMX8QXP_UART1_RTS_B_LSIO_PWM2_OUT               0x60>;
        };
}
&pwm2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pwm2_d>;
#pwm-cells = <2>;
status = "okay";
};
0 Kudos
Reply
1 Reply

913 Views
igorpadykov
NXP Employee
NXP Employee

Hi ABHISHEK

 

for pwm2 example one can look on

https://community.nxp.com/t5/i-MX-Processors/Yocto-3-0-imx8qxp-support-pwm2/m-p/1329148#M179046

 

Best regards
igor

0 Kudos
Reply