hi
this is saida
wordking on custmoised i.mx6 board
i am using ARM DS5 and Dstream for code development,debugging respectively
i am facing one problem
i have one application code which running with debugger perfectly but
the same bin file when i am running from u-boot with loadb command
its not running and it is going to SVC,UNDEF,ABORT handlers
the code is given below
/*******************************************/
struct t1
{
float x;
int y;
};
typedef struct t1 t1struct;
struct six
{
float xx;
int yy;
t1struct xyz;
boolean v;
};
typedef struct six sixstruct;
void datacopy(t1struct *T)
{
T->y =1;
}
void start(sixstruct *data)
{
datacopy(&(data->xyz));
}
int main(void)
{
sixstruct s;
start(&s);
return EXIT_SUCCESS;
}
/******************************************/
please can any one help me in this regard
thanks in advance
regards
Saida