problem facing for making hello application through ltib

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem facing for making hello application through ltib

2,870 Views
HimanshuDobhal
Contributor I

Processing platform: Freescale iMX5x Based Boards
===================================================
using config/platform/imx/.config

Processing: hello
===================
dropping %{hello} in spec token: sources
dropping %{1.0} in spec token: sources
Build path taken because: no prebuilt rpm,
Testing network connectivity
OK GPP:

Try -.tar.bz2.md5 from the GPP
http://bitshrine.org/gpp/-.tar.bz2.md5:
00:03:44 ERROR 404: Not Found.
Try -.tar.bz2 from the GPP
http://bitshrine.org/gpp/-.tar.bz2:
00:03:44 ERROR 404: Not Found.
Can't get: -.tar.bz2 at ./ltib line 790.


f_buildrpms() returned an error, exiting
traceback:
 main:560


Started: Wed Apr 11 00:03:35 2012
Ended:   Wed Apr 11 00:03:44 2012
Elapsed: 9 seconds

These packages failed to build:
hello

Build Failed

Exiting on error or interrupt

Can any one have idea about this problem as i am not able to rectifying that what is the problem

Tags (2)
0 Kudos
Reply
4 Replies

2,631 Views
daiane_angolini
NXP Employee
NXP Employee

LTIB is trying to donwload the file -.tar.bz2 instead of YOURAPPLICATION-VERSION.tar.bz2, look:

Try -.tar.bz2.md5 from the GPP

http://bitshrine.org/gpp/-.tar.bz2.md5:

00:03:44 ERROR 404: Not Found.

Try -.tar.bz2 from the GPP

http://bitshrine.org/gpp/-.tar.bz2:

00:03:44 ERROR 404: Not Found.

Can't get: -.tar.bz2 at ./ltib line 790.


Change the name of your application on your spec file.


For u-boot, I would suggest you to build it manually, without LTIB. It's easier.


0 Kudos
Reply

2,631 Views
Balaji_ng
Contributor III

Hi,

     Check your spec file. This seems to be a problem with your spec file.

Hope this helps.

Regards,

Balaji.V

0 Kudos
Reply

2,631 Views
Vijayaragavan
Contributor I

Hi balaji,

# template = u-boot-common.tmpl

%define pfx /opt/freescale/rootfs/%{_target_cpu}

Summary         : Universal Bootloader firmware

Name            : u-boot

Version         : 2009.08

Release         : imx_09.12.01

License         : GPL

Vendor          : Freescale

Packager        : MAD

Group           : Applications/System

Source          : %{name}-%{version}.tar.bz2

Source1         : %{name}-v%{version}-%{release}.tar.bz2

BuildRoot       : %{_tmppath}/%{name}

Prefix          : %{pfx}

%Description

%{summary}

Open source u-boot v2009.08 version

%Prep

%setup

# A single bz2 file contains all the patches and a series file.

tar jxvf %{SOURCE1}

chmod 755 patches/patch-uboot.sh

./patches/patch-uboot.sh

%Build

: ${PKG_U_BOOT_CONFIG_TYPE:?must be set, e.g. MPC8548CDS_config}

PKG_U_BOOT_PATH_PRECONFIG=$(eval echo $PKG_U_BOOT_PATH_PRECONFIG)

SRC_DIR=${PKG_U_BOOT_PATH_PRECONFIG:-%{_builddir}/%{buildsubdir}}

%{!?showsrcpath: %define showsrcpath 0}

%if %{showsrcpath}

%{echo:%(eval echo ${PKG_U_BOOT_PATH_PRECONFIG:-%{_builddir}/%{buildsubdir}})}

%endif

BUILD_DIR=%{_builddir}/%{buildsubdir}

if [ $SRC_DIR != $BUILD_DIR ]

then

    mkdir -p $BUILD_DIR

fi

cd $SRC_DIR

if [ -n "$LTIB_FULL_REBUILD" ]

then

    make HOSTCC="$BUILDCC" CROSS_COMPILE=$TOOLCHAIN_PREFIX O=$BUILD_DIR distclean

fi

make HOSTCC="$BUILDCC" CROSS_COMPILE=$TOOLCHAIN_PREFIX O=$BUILD_DIR $PKG_U_BOOT_CONFIG_TYPE

make HOSTCC="$BUILDCC" HOSTSTRIP="$BUILDSTRIP" \

     CROSS_COMPILE=$TOOLCHAIN_PREFIX $PKG_U_BOOT_BUILD_ARGS \

     O=$BUILD_DIR all

%Install

rm -rf $RPM_BUILD_ROOT

mkdir -p $RPM_BUILD_ROOT/%{pfx}/boot

BUILD_DIR=%{_builddir}/%{buildsubdir}

cd $BUILD_DIR

for i in u-boot.bin u-boot

do

    cp $i $RPM_BUILD_ROOT/%{pfx}/boot

done

%Clean

rm -rf $RPM_BUILD_ROOT

%Files

%defattr(-,root,root)

%{pfx}/*

this is what my uboot.spec file content. what to change and where to change?

0 Kudos
Reply

2,631 Views
hyejinyang
Contributor I

in which place is this spec file?

0 Kudos
Reply