porting android to new board - init: cannot find '/system/bin/sh', disabling 'console'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

porting android to new board - init: cannot find '/system/bin/sh', disabling 'console'

Jump to solution
9,513 Views
varsmolta
Contributor V

I have a RM3 board from bluechip technologies. I've been able to port u-boot and kernel to it, using the boundary devices android builds as a guide. I am using the boundary devices android filesystem images as well with my modified kernel. When booting android 4.0.4, I get the following error:

init: property (null) has no value for writing to /sys/class/android_usb/android0/iManufacturer

init: property (null) has no value for writing to /sys/class/android_usb/android0/iProduct

init: cannot find '/system/bin/sh', disabling 'console'

init: cannot find '/system/bin/servicemanager', disabling 'servicemanager'

init: cannot find '/system/bin/vold', disabling 'vold'

init: cannot find '/system/bin/gpu_init.sh', disabling 'gpu_init'

init: cannot find '/system/bin/netd', disabling 'netd'

init: cannot find '/system/bin/dispd', disabling 'dispd'

init: cannot find '/system/bin/debuggerd', disabling 'debuggerd'

init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger'

init: cannot find '/system/bin/app_process', disabling 'zygote'

init: cannot find '/system/bin/drmserver', disabling 'drm'

init: cannot find '/system/bin/mediaserver', disabling 'media'

init: cannot find '/system/bin/dbus-daemon', disabling 'dbus'

init: cannot find '/system/bin/installd', disabling 'installd'

init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'

init: cannot find '/system/bin/keystore', disabling 'keystore'

init: cannot find '/system/bin/rild', disabling 'ril-daemon'

init: cannot find '/system/bin/sh', disabling 'console'

From reading online in the forums, it seems I may not be loading the filesystem correctly. Can anyone please guide me on how to tackle this problem?

Here is the full bootlog (note: even though it says Sabre Lite in many places, this is really the RM3 board. I have tweaked u-boot and kernel to accommodate for the RM3):

U-Boot 2009.08-dirty (Jun 28 2014 - 20:32:38)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz

Temperature:   47 C, calibration data 0x5704c47d

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock     : 66000000Hz

ipg per clock : 66000000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 132000000Hz

axi clock   : 264000000Hz

emi_slow clock: 29333333Hz

ddr clock     : 528000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

nfc clock     : 24000000Hz

Board: MX6Q-SABRELITE:[ POR]

Boot Device: NOR

I2C:   ready

DRAM:   1 GB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1

JEDEC ID: 0xbf:0x25:0x8e

Reading SPI NOR flash 0xc0000 [0x2000 bytes] -> ram 0x27600a18

SUCCESS

In:    serial

Out:   serial

Err:   serial

Net:   got MAC address from IIM: 00:c0:46:00:88:f1

FEC0 [PRIME]

Hit any key to stop autoboot:  0

MX6Q SABRELITE U-Boot > mmc dev 0

mmc0 is current device

MX6Q SABRELITE U-Boot > mmc rescan; fatload mmc 0:1 ${loadaddr} uImage && fatload mmc 0:1 12800000 uramdisk.img && bootm 10800000 12800000

reading uImage

4354968 bytes read

reading uramdisk.img

213592 bytes read

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35-gb8823c8-dirty

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    4354904 Bytes =  4.2 MB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 12800000 ...

   Image Name:   Initial Ram Disk

   Image Type:   ARM Linux RAMDisk Image (gzip compressed)

   Data Size:    213528 Bytes = 208.5 kB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Starting kernel ...

Initializing cgroup subsys cpuset

Initializing cgroup subsys cpu

Linux version 3.0.35-gb8823c8-dirty (ashwin@ashwin1) (gcc version 4.7.1 20120531 (prerelease) (crosstool-NG linaro-1.13.1-2012.06-20120625 - Linaro GCC 2012.06) ) #13 SMP PREEMPT Sun J

un 29 20:00:55 EDT 2014

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX 6Quad Sabre-Lite Board

Memory policy: ECC disabled, Data cache writealloc

CPU identified as i.MX6Q, silicon rev 1.2

PERCPU: Embedded 7 pages/cpu @c1174000 s5760 r8192 d14720 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 210944

Kernel command line: enable_wait_mode=off console=ttymxc0,115200 vmalloc=400M consoleblank=0 video=mxcfb0:dev=lcd,DTECH,if=RGB666 fbmem=10M androidboot.bootdev=sdhci-esdhc-imx.0 androi

dboot.hardware=freescale androidboot.console=ttymxc0

PID hash table entries: 2048 (order: 1, 8192 bytes)

Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

Memory: 576MB 256MB = 832MB total

Memory: 833424k/833424k available, 215152k reserved, 442368K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xfbe00000 - 0xffe00000   (  64 MB)

    vmalloc : 0xd9800000 - 0xf2000000   ( 392 MB)

    lowmem  : 0xc0000000 - 0xd9000000   ( 400 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .init : 0xc0008000 - 0xc0041000   ( 228 kB)

      .text : 0xc0041000 - 0xc07cf458   (7738 kB)

      .data : 0xc07d0000 - 0xc083a060   ( 425 kB)

       .bss : 0xc083a084 - 0xc096a820   (1218 kB)

Preemptible hierarchical RCU implementation.

NR_IRQS:624

MXC GPIO hardware

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

MXC_Early serial console at MMIO 0x2020000 (options '115200')

bootconsole [ttymxc0] enabled

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Initializing cgroup subsys cpuacct

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

CPU1: Booted secondary processor

Brought up 2 CPUs

SMP: Total of 2 processors activated (3162.11 BogoMIPS).

print_constraints: dummy:

NET: Registered protocol family 16

print_constraints: vddpu: 725 <--> 1300 mV at 1150 mV fast normal

print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal

print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal

print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal

print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

------------ Board type Sabre Lite

imx_add_mxc_pwm:pdata=  (null)

imx_add_mxc_pwm:pdata=  (null)

imx_add_mxc_pwm:pdata=  (null)

imx_add_mxc_pwm:pdata=  (null)

hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.

hw-breakpoint: maximum watchpoint size is 4 bytes.

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B

IMX usb wakeup probe

bio: create slab <bio-0> at 0

print_constraints: VDDA: 2500 mV

print_constraints: VDDIO: 3300 mV

machine_constraints_voltage: VDDD: unsupportable voltage constraints

reg-fixed-voltage reg-fixed-voltage.2: Failed to register regulator: -22

reg-fixed-voltage: probe of reg-fixed-voltage.2 failed with error -22

print_constraints: vmmc: 3300 mV

vgaarb: loaded

SCSI subsystem initialized

spi_imx imx6q-ecspi.0: probed

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Freescale USB OTG Driver loaded, $Revision: 1.55 $

add wake up source irq 75

imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed

mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Version 1.0.24.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

cfg80211: Calling CRDA to update world regulatory domain

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

IP route cache hash table entries: 16384 (order: 4, 65536 bytes)

TCP established hash table entries: 65536 (order: 7, 524288 bytes)

TCP bind hash table entries: 65536 (order: 7, 786432 bytes)

TCP: Hash tables configured (established 65536 bind 65536)

TCP reno registered

UDP hash table entries: 256 (order: 1, 8192 bytes)

UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Unpacking initramfs...

Freeing initrd memory: 208K

Static Power Management for Freescale i.MX6

wait mode is disabled for i.MX6

cpaddr = d9880000 suspend_iram_base=d9918000

PM driver module loaded

IMX usb wakeup probe

i.MXC CPU frequency driver

highmem bounce pool size: 64 pages

ashmem: initialized

JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

msgmni has been set to 764

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

pwm_config: pwm freq = 32786, clk_select=2 clock_rate=6000000

pwm_config: pwm freq = 20000, clk_select=2 clock_rate=6000000

MIPI DSI driver module loaded

mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver lcd

pwm_config: pwm freq = 32786, clk_select=2 clock_rate=6000000

pwm_config: pwm freq = 20000, clk_select=2 clock_rate=6000000

mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver lcd

mxc_sdc_fb mxc_sdc_fb.1: ipu0-di0 already in use

mxc_sdc_fb: probe of mxc_sdc_fb.1 failed with error -16

mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver ldb

_regulator_get: get() with no identifier

imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

pwm_config: pwm freq = 32786, clk_select=2 clock_rate=6000000

pwm_config: pwm freq = 20000, clk_select=2 clock_rate=6000000

mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb

pwm_config: pwm freq = 32786, clk_select=2 clock_rate=6000000

pwm_config: pwm freq = 20000, clk_select=2 clock_rate=6000000

imx-sdma imx-sdma: loaded firmware 1.1

imx-sdma imx-sdma: initialized

Serial: IMX driver

imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

console [ttymxc0] enabled, bootconsole disabled

console [ttymxc0] enabled, bootconsole disabled

imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX

loop: module loaded

Can't recover from RESET HBA!

No sata disk.

m25p80 spi0.0: found sst25vf080b, expected sst25vf016b

m25p80 spi0.0: sst25vf080b (1024 Kbytes)

Creating 3 MTD partitions on "m25p80":

0x000000000000-0x0000000c0000 : "bootloader"

0x0000000c0000-0x0000000c2000 : "ubparams"

0x0000000c2000-0x000000100000 : "unused"

vcan: Virtual CAN interface driver

CAN device driver interface

flexcan netdevice driver

FEC Ethernet Driver

fec_enet_mii_bus: probed

PPP generic driver version 2.4.2

PPP Deflate Compression module registered

PPP BSD Compression module registered

PPP MPPE Compression module registered

NET: Registered protocol family 24

PPTP driver version 0.8.5

tun: Universal TUN/TAP device driver, 1.6

tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

add wake up source irq 72

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

usbcore: registered new interface driver cdc_acm

cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

usbcore: registered new interface driver usbserial

usbserial: USB Serial Driver core

USB Serial support registered for GSM modem (1-port)

usbcore: registered new interface driver option

option: v0.7.2:USB Driver for GSM modems

USB Serial support registered for Qualcomm USB modem

usbcore: registered new interface driver qcserial

ARC USBOTG Device Controller driver (1 August 2005)

android_usb gadget: Mass Storage Function, version: 2009/09/11

android_usb gadget: Number of LUNs=1

lun0: LUN: removable file: (no medium)

Gadget Android: controller 'fsl-usb2-udc' not recognized

android_usb gadget: android_usb ready

Suspend udc for OTG auto detect

fsl-usb2-udc: bind to driver android_usb

mousedev: PS/2 mouse device common for all mice

input: gpio-keys as /devices/platform/gpio-keys/input/input0

tsc2004_prepare_for_reading: write_cmd -5

tsc2004: probe of 2-0048 failed with error -5

egalax_ts 2-0004: egalax_ts: failed to read firmware version

egalax_ts: probe of 2-0004 failed with error -5

ft5x06-ts 2-0038: ft5x06: Could not detect touch screen.

ft5x06: Jun 28 2014

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

using rtc device, snvs_rtc, for alarms

snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0

i2c /dev entries driver

Linux video capture interface: v2.00

ov5642_read_reg:write reg error:reg=300a

ov5642_probe:cannot find camera

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20

usbcore: registered new interface driver uvcvideo

usb 2-1: new high speed USB device number 2 using fsl-ehci

USB Video Class driver (v1.1.0)

i2c-core: driver [mag3110] using legacy suspend method

android_work: did not send uevent (0 0   (null))

i2c-core: driver [mag3110] using legacy resume method

imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCILL protocol initialized

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

mmc0: no vmmc regulator found

mmc0: SDHCI controller on platform [sdhci-esdhc-imx.0] using DMA

sdhci sdhci-esdhc-imx.2: no write-protect pin available!

sdhci sdhci-esdhc-imx.2: no card-detect pin available!

mmc1: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA

mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

VPU initialized

mxc_asrc registered

revserved_memory_account:viv_gpu registerd

anatop_thermal anatop_thermal.0: fuse data: 0x5704c47d

Thermal calibration data is 0x5704c47d

anatop_thermal_counting_ratio: raw25c=1392 raw_hot=1220 hot_temp=125

android_work: sent uevent USB_STATE=CONNECTED

android_work: sent uevent USB_STATE=DISCONNECTED

Anatop Thermal registered as thermal_zone0

anatop_thermal_probe: default cooling device is cpufreq!

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

logger: created 256K log 'log_main'

logger: created 256K log 'log_events'

logger: created 256K log 'log_radio'

logger: created 256K log 'log_system'

usbcore: registered new interface driver snd-usb-audio

mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio

imx-hdmi-soc-dai: probe of imx-hdmi-soc-dai.0 failed with error -12

sgtl5000 0-000a: Failed to get supply 'VDDD': -19

print_constraints: 0-000a: 850 <--> 1600 mV at 1200 mV normal

sgtl5000 0-000a: Device with ID register 0 is not a sgtl5000

sgtl5000 0-000a: asoc: failed to probe CODEC sgtl5000.0-000a: -19

asoc: failed to instantiate card sgtl5000-audio: -19

ALSA device list:

  No soundcards found.

Netfilter messages via NETLINK v0.30.

nf_conntrack version 0.5.0 (13025 buckets, 52100 max)

ctnetlink v0.93: registering with nfnetlink.

mmc0: new high speed SDHC card at address aaaa

NF_TPROXY: Transparent proxy support initialized, version 4.1.0

NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.

mmcblk0: mmc0:aaaa SL16G 14.8 GiB (ro)

xt_time: kernel timezone is -0000

IPv4 over IPv4 tunneling driver

GRE over IPv4 demultiplexor driver

ip_tables: (C) 2000-2006 Netfilter Core Team

arp_tables: (C) 2002 David S. Miller

TCP cubic registered

NET: Registered protocol family 10

mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4

ip6_tables: (C) 2000-2006 Netfilter Core Team

IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

NET: Registered protocol family 15

can: controller area network core (rev 20090105 abi 8)

android_work: sent uevent USB_STATE=CONNECTED

NET: Registered protocol family 29

can: raw protocol (rev 20090105)

can: broadcast manager protocol (rev 20090105 t)

android_work: sent uevent USB_STATE=DISCONNECTED

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

L2TP core driver, V2.0

PPPoL2TP kernel driver, V2.0

L2TP IP encapsulation support (L2TPv3)

L2TP netlink interface

L2TP ethernet pseudowire support (L2TPv3)

lib80211: common routines for IEEE802.11 drivers

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

Bus freq driver module loaded

Bus freq driver Enabled

mxc_dvfs_core_probe

DVFS driver module loaded

regulator_init_complete: VDDIO: incomplete constraints, leaving on

regulator_init_complete: VDDA: incomplete constraints, leaving on

snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)

Freeing init memory: 228K

init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.

android_work: sent uevent USB_STATE=CONNECTED

android_work: sent uevent USB_STATE=DISCONNECTED

usb 2-1: device not accepting address 2, error -71

usb 2-1: new high speed USB device number 3 using fsl-ehci

android_work: sent uevent USB_STATE=CONNECTED

init: cannot open '/initlogo.rle'

init: command 'loglevel' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'export' r=0

init: command 'symlink' r=0

init: command 'symlink' r=0

init: command 'symlink' r=0

hub 2-1:1.0: USB hub found

init: command 'mkdir' r=0

hub 2-1:1.0: 2 ports detected

init: command 'mount' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'symlink' r=0

init: command 'mkdir' r=0

init: command 'symlink' r=0

init: command 'mkdir' r=0

init: command 'symlink' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mount' r=0

init: command 'mkdir' r=0

init: command 'mount' r=0

init: command 'mkdir' r=0

init: command 'mount' r=0

init: command 'write' r=0

init: command 'write' r=-2

init: command 'write' r=0

init: command 'write' r=-2

init: command 'write' r=-2

init: command 'write' r=-2

init: command 'write' r=0

init: command 'write' r=0

init: command 'mkdir' r=0

init: command 'mount' r=0

init: command 'chown' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'write' r=-22

init: command 'mkdir' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'write' r=0

init: command 'mkdir' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'write' r=0

init: command 'chmod' r=0

init: processing action 0x31fe0 (fs)

init: command 'mount' r=-1

init: command 'mount' r=0

init: command 'mount' r=-1

init: command 'mkdir' r=0

init: command 'mount' r=-1

init: executing '/sbin/ts_calibrator'

init: executed '/sbin/ts_calibrator' done

init: command 'exec' r=0

init: processing action 0x2b080 (post-fs)

init: command 'mount' r=0

init: command 'chown' r=-30

init: command 'chmod' r=-30

init: command 'chown' r=-2

init: command 'chmod' r=-2

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'mkdir' r=-30

init: processing action 0x2b2a0 (post-fs-data)

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'mkdir' r=0

init: command 'copy' r=-1

init: command 'chown' r=-2

init: command 'chmod' r=-2

init: command 'copy' r=-1

init: command 'chown' r=-2

init: command 'chmod' r=-2

init: command 'write' r=-2

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'chmod' r=0

init: command 'chmod' r=-2

init: command 'chmod' r=-2

init: command 'chmod' r=-2

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'chmod' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: processing action 0x32438 (property_service_init)

init: Created socket '/dev/socket/property_service' with mode '666', user '0', group '0'

init: command 'property_service_init' r=0

init: processing action 0x32480 (signal_init)

init: command 'signal_init' r=0

init: processing action 0x324c8 (check_startup)

init: command 'check_startup' r=0

init: processing action 0x2ba10 (boot)

init: command 'ifup' r=0

init: command 'hostname' r=0

init: command 'domainname' r=0

init: command 'setrlimit' r=0

init: command 'write' r=0

init: command 'write' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'write' r=0

init: command 'write' r=0

init: command 'write' r=0

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=0

init: command 'chown' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chmod' r=0

init: command 'chmod' r=0

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=0

init: command 'chown' r=0

init: command 'chown' r=0

init: command 'chown' r=0

init: command 'chown' r=0

init: command 'chown' r=0

init: command 'chown' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'chown' r=0

init: command 'chmod' r=-2

init: command 'chown' r=-2

init: command 'write' r=-2

init: command 'write' r=0

init: property (null) has no value for writing to /sys/class/android_usb/android0/iManufacturer

init: command 'write' r=-22

init: property (null) has no value for writing to /sys/class/android_usb/android0/iProduct

init: command 'write' r=-22

init: command 'write' r=0

init: command 'mount' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: cannot find '/system/bin/sh', disabling 'console'

init: cannot find '/system/bin/servicemanager', disabling 'servicemanager'

init: cannot find '/system/bin/vold', disabling 'vold'

init: cannot find '/system/bin/gpu_init.sh', disabling 'gpu_init'

init: command 'class_start' r=0

init: cannot find '/system/bin/netd', disabling 'netd'

init: cannot find '/system/bin/dispd', disabling 'dispd'

init: cannot find '/system/bin/debuggerd', disabling 'debuggerd'

init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger'

init: cannot find '/system/bin/app_process', disabling 'zygote'

init: cannot find '/system/bin/drmserver', disabling 'drm'

init: cannot find '/system/bin/mediaserver', disabling 'media'

init: cannot find '/system/bin/dbus-daemon', disabling 'dbus'

init: cannot find '/system/bin/installd', disabling 'installd'

init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'

init: cannot find '/system/bin/keystore', disabling 'keystore'

init: cannot find '/system/bin/rild', disabling 'ril-daemon'

init: command 'class_start' r=0

init: processing action 0x313b8 (boot)

init: command 'symlink' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'setprop' r=0

init: command 'chown' r=0

init: command 'chown' r=0

init: command 'chown' r=-2

init: command 'chown' r=-2

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chmod' r=0

init: command 'chmod' r=0

init: command 'chmod' r=-2

init: command 'chmod' r=-2

init: command 'chmod' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chown' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chown' r=-2

init: command 'chmod' r=-2

init: command 'chown' r=-2

init: command 'chmod' r=-2

init: command 'setprop' r=0

init: command 'chown' r=0

init: command 'chmod' r=0

init: command 'chmod' r=0

init: command 'chmod' r=0

init: command 'write' r=0

init: command 'write' r=0

init: command 'write' r=0

init: command 'write' r=0

init: command 'write' r=0

init: command 'write' r=0

init: command 'chmod' r=0

init: command 'chmod' r=0

init: command 'chmod' r=0

init: command 'chmod' r=0

init: command 'chmod' r=0

init: command 'chmod' r=0

init: command 'mkdir' r=-2

init: command 'chmod' r=-2

init: command 'chmod' r=-2

init: command 'chown' r=-2

init: command 'mkdir' r=0

init: command 'mkdir' r=0

init: command 'chmod' r=0

init: command 'chmod' r=-2

init: command 'chown' r=0

init: command 'chown' r=-2

init: command 'setprop' r=0

init: processing action 0x32510 (queue_propety_triggers)

init: command 'queue_propety_triggers' r=0

init: processing action 0x2d120 (property:persist.sys.usb.config=*)

init: command 'setprop' r=0

init: processing action 0x2d3f0 (property:ro.debuggable=1)

init: cannot find '/system/bin/sh', disabling 'console'

init: command 'start' r=0

init: starting 'adbd'

init: command 'start' r=0

adb_open

init: processing action 0x31018 (property:sys.usb.config=mtp,adb)

android_usb: already disabled

init: command 'write' r=0

init: command 'write' r=0

init: command 'write' r=0

init: command 'write' r=0

mtp_bind_config

adb_bind_config

init: command 'write' r=0

init: command 'start' r=0

init: command 'setprop' r=0

android_work: sent uevent USB_STATE=DISCONNECTED

android_work: sent uevent USB_STATE=CONNECTED

android_usb gadget: high speed config #1: android

android_work: sent uevent USB_STATE=CONFIGURED

Labels (5)
0 Kudos
Reply
1 Solution
3,757 Views
varsmolta
Contributor V

Had to change vold.fstab file to mount the correct sd card device

this line:

dev_mount sdcard /mnt/sdcard 4 /devices/platform/sdhci-esdhc-imx.0/mmc_host/mmc1

where sdhci-esdhc-imx.x is the sd card platform device number

View solution in original post

0 Kudos
Reply
2 Replies
3,757 Views
varsmolta
Contributor V

Also, if I adb shell, I get this:

- exec '/system/bin/sh' failed: No such file or directory (2) -

and

adb ls /system gives this:

000041ed 00000000 53b0e158 .

000041fd 00000000 00000001 ..

0 Kudos
Reply
3,758 Views
varsmolta
Contributor V

Had to change vold.fstab file to mount the correct sd card device

this line:

dev_mount sdcard /mnt/sdcard 4 /devices/platform/sdhci-esdhc-imx.0/mmc_host/mmc1

where sdhci-esdhc-imx.x is the sd card platform device number

0 Kudos
Reply