populate_sdk failed on imx8mplus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

populate_sdk failed on imx8mplus

938 次查看
Eddy1
Contributor V

HI:

I am trying to generate the SDK with the following modifications:

  1. Comment out the following two lines as shown below:

Eddy1_0-1697108658885.png

2.The command execution is resulting in an error.

bitbake -c populate_sdk meta-toolchain-qt5

 

 util-linux-ul                                                            cortexa53_crypto           2.36-r0                              oe-repo   13 k
 util-linux-unshare                                                       cortexa53_crypto           2.36-r0                              oe-repo   21 k
 util-linux-utmpdump                                                      cortexa53_crypto           2.36-r0                              oe-repo   15 k
 util-linux-uuidd                                                         cortexa53_crypto           2.36-r0                              oe-repo   19 k
 util-linux-uuidgen                                                       cortexa53_crypto           2.36-r0                              oe-repo   11 k
 util-linux-uuidparse                                                     cortexa53_crypto           2.36-r0                              oe-repo   19 k
 util-linux-wall                                                          cortexa53_crypto           2.36-r0                              oe-repo   18 k
 util-linux-wdctl                                                         cortexa53_crypto           2.36-r0                              oe-repo   26 k
 util-linux-whereis                                                       cortexa53_crypto           2.36-r0                              oe-repo   16 k
 util-linux-wipefs                                                        cortexa53_crypto           2.36-r0                              oe-repo   21 k
 util-linux-write                                                         cortexa53_crypto           2.36-r0                              oe-repo   12 k
 util-linux-zramctl                                                       cortexa53_crypto           2.36-r0                              oe-repo   45 k
 util-macros-dev                                                          cortexa53_crypto           1:1.19.2-r0                          oe-repo   22 k
 valgrind-dev                                                             cortexa53_crypto           3.16.1-r0                            oe-repo  290 k
 volatile-binds-dev                                                       noarch                     1.0-r0                               oe-repo  5.7 k
 vulkan-headers-dev                                                       cortexa53_crypto           1.1.121-r0                           oe-repo  259 k
 wayland-dev                                                              cortexa53_crypto           1.19.0-r0                            oe-repo   61 k
 which-dev                                                                cortexa53_crypto           2.21-r3                              oe-repo  6.0 k
 wireless-tools                                                           cortexa53_crypto           1:30.pre9-r0                         oe-repo   42 k
 wpa-supplicant-cli                                                       cortexa53_crypto           2.9-r0                               oe-repo   47 k
 wpa-supplicant-passphrase                                                cortexa53_crypto           2.9-r0                               oe-repo   28 k
 xcb-proto-dev                                                            cortexa53_crypto           1.14-r0                              oe-repo   81 k
 xf86-input-libinput                                                      cortexa53_crypto           2:0.30.0-r0                          oe-repo   31 k
 xkbcomp                                                                  cortexa53_crypto           1.4.3-r0                             oe-repo   79 k
 xkeyboard-config-dev                                                     cortexa53_crypto           2.30-r0                              oe-repo  7.0 k
 xorgproto-dev                                                            cortexa53_crypto           2020.1-r0                            oe-repo  173 k
 xrandr-dev                                                               cortexa53_crypto           1:1.5.1-r0                           oe-repo  6.0 k
 xserver-xf86-config                                                      myd_jx8mp                  0.1-r33                              oe-repo  6.4 k
 xtrans-dev                                                               cortexa53_crypto           1:1.4.0-r0                           oe-repo   42 k
 xz-dev                                                                   cortexa53_crypto           5.2.5-r0                             oe-repo   42 k

Transaction Summary
========================================================================================================================================================
Install 2459 Packages

Total size: 911 M
Installed size: 3.2 G
Downloading Packages:
Running transaction check
Transaction check succeeded.
Running transaction test
Error: Transaction test error:
file /etc/default/weston conflicts between attempted installs of nxp-demo-experience-1.0-r0.cortexa53_crypto and weston-init-1.0-r0.

Please give me advise?

0 项奖励
回复
1 回复

910 次查看
Harvey021
NXP TechSupport
NXP TechSupport

It is better not to comment out the default settings.

 

Best regards

Harvey

0 项奖励
回复