pinnmux in imx8m

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

pinnmux in imx8m

跳至解决方案
1,829 次查看
yashavanthashet
Contributor V

Hi ,

Can anyone let me know what are below tuples used in "pins-imx8mq.h" file?

"<mux_reg conf_reg input_reg mux_mode input_val>"

I have understood that mux_reg  is offset of mux reg and conf_reg is offset of pad reg, and also mux_mode is alt-mode used.

But what are input_reg and input_val?

Also let me know how values to particular pins are given in dts?

for example in below pins how 82 is decided?

MX8MQ_IOMUXC_ECSPI1_SCLK_ECSPI1_SCLK    0x82

Thanks and Regards,

Yashavantha

0 项奖励
回复
1 解答
1,573 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yashavantha

these are input daisy register, for example

#define MX8MQ_IOMUXC_GPIO1_IO11_CCMSRCGPCMIX_PMIC_READY    0x054 0x2BC 0x4BC 0x5 0x1

nput_reg = 0x4BC - INPUT DAISY Register
input_val  = 0x1

sect.8.2.4.299 CCM_PMIC_READY_SELECT_INPUT DAISY Register
(IOMUXC_CCM_PMIC_READY_SELECT_INPUT) i.MX8MDQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

>for example in below pins how 82 is decided?

>MX8MQ_IOMUXC_ECSPI1_SCLK_ECSPI1_SCLK    0x82

this is setting for IOMUXC_SW_PAD_CTL_PAD_ECSPI1_SCLK described in

sect.8.2.4.275 SW_PAD_CTL_PAD_ECSPI1_SCLK SW PAD Control
Register (IOMUXC_SW_PAD_CTL_PAD_ECSPI1_SCLK) i.MX8MDQ Reference Manual 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,574 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yashavantha

these are input daisy register, for example

#define MX8MQ_IOMUXC_GPIO1_IO11_CCMSRCGPCMIX_PMIC_READY    0x054 0x2BC 0x4BC 0x5 0x1

nput_reg = 0x4BC - INPUT DAISY Register
input_val  = 0x1

sect.8.2.4.299 CCM_PMIC_READY_SELECT_INPUT DAISY Register
(IOMUXC_CCM_PMIC_READY_SELECT_INPUT) i.MX8MDQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

>for example in below pins how 82 is decided?

>MX8MQ_IOMUXC_ECSPI1_SCLK_ECSPI1_SCLK    0x82

this is setting for IOMUXC_SW_PAD_CTL_PAD_ECSPI1_SCLK described in

sect.8.2.4.275 SW_PAD_CTL_PAD_ECSPI1_SCLK SW PAD Control
Register (IOMUXC_SW_PAD_CTL_PAD_ECSPI1_SCLK) i.MX8MDQ Reference Manual 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------