Hello.,.,
Board Detail : imx6 Sabre SD board (Imx6q processor)
I am trying to load standalone program (hello_world.bin) which is available in u-boot source code folder,but after running standalone code board is getting RESET, I have done few modification in u-boot source code
In /arch/arm/config.mk file CONFIG_STANDALONE_LOAD_ADDR has been modified to 0x12000000
also In include/configs/mx6_common.h CONFIG_LOADADDR has been modified to 0x12000000.
I am using SD Card to load bin file to RAM . and using GO command. Can anyone suggest where I am doing mistake, is there any steps I missing.
My u-boot command prompt LOG
=>
U-Boot SPL 2018.09-rc2-00140-g11ed312-dirty (Aug 29 2018 - 18:25:28 +0530)
Trying to boot from MMC1
U-Boot 2018.09-rc2-00140-g11ed312-dirty (Aug 29 2018 - 18:25:28 +0530)
CPU: Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)
CPU: Automotive temperature grade (-40C to 125C) at 43C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... OK
PCI: pcie phy link never came up
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Net: FEC [PRIME]
Hit any key to stop autoboot: 0
=>
=> fatls mmc 1:2 /
578 hello_world.bin
.Trash-1000/
1 file(s), 1 dir(s)
=> fatload mmc 1:2 0x12000000 hello_world.bin
578 bytes read in 14 ms (40 KiB/s)
=>
=> go 0x12000000 this is test
## Starting application at 0x12000000 ...
undefined instruction
pc : [<12000010>] lr : [<4ff69bcf>]
reloc pc : [<d989a010>] lr : [<17803bcf>]
sp : 4f565d48 ip : 0000001c fp : 00000005
r10: 4ffc44d0 r9 : 4f565ea0 r8 : 4f568938
r7 : 4ff69ba5 r6 : 00000005 r5 : 12000000 r4 : 4f56893c
r3 : 12000000 r2 : 4f56893c r1 : 4f56893c r0 : fffff9f6
Flags: nzCv IRQs off FIQs off Mode SVC_32
Code: 41f0e92d 46084605 2400460e f8c6f000 (21094f17)
Resetting CPU ...
resetting ...
U-Boot SPL 2018.09-rc2-00140-g11ed312-dirty (Aug 29 2018 - 18:25:28 +0530)
Trying to boot from MMC1
Thank you.,.,
Hello
I apologize for the late answer.
Can you please tell me which BSP are you using. I will try to reproduce the error on my board.
Best Regards,
Diego.