Hi all,
I've tried to install imagemagick on linux imx6 baseline.
So, i added x11 and perl packages. But when installing imagemagick package, there's the following error:
/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find -lperl
I can see perl-5.8.8-2 package is installed but it seems to me i should see other entries like libperl-dev ,...
I suppose perl package is not enough.
Does someone know what packages profile to use ?
Rgds,
Christophe
the -dev package is usually for headers files, needed for development. Is libperl.so somewhere on your filesystem? if yes, you may use the -L to indicate the folder where it resides.
 
					
				
		
In ltib/rootfs/usr/lib, i've a perl5 directory with many directories and .pm files. But i can't locate libperl.so wheter in perl5 or another lib directory.
 
					
				
		
Chris
This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.
Thanks,
Yixing
 
					
				
		
Chris
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing