Hello,
When I am booting up the i.MX53 SABRE tablet with Ubuntu 10.04 LTS I am noticing that most of delay during boot up is because of sending client DHCP request and waiting for the timeout to expire. The exact message is (also see attachment):
Sending DHCP requests ...... timed out!
IP-Config: Reopening network devices...
eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=0:00, irq=-1)
Sending DHCP requests ...... timed out!
The boot time takes about 3 minutes 26 seconds. Majority of the time, about 2 minutes is because of the DHCP timeout. How can I modify this timeout to be on the order of 5-10 seconds instead of two minutes?
Sincerely,
Kris