opencv 4.5.5 failed with do_package_qa error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

opencv 4.5.5 failed with do_package_qa error

975件の閲覧回数
vsuneja63
Contributor III

Hi,

I am building yocto kirkston sources for imx8mq platform. It's throwing opencv fatal QA error, here are the logs:

vipulkumar@A812DBLR:~/platform/AGL_Needlefish/build$ bitbake -k agl-demo-platform
WARNING: DISTRO_FEATURES:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
Loading cache: 100% | | ETA: --:--:--
Loaded 0 entries from dependency cache.
WARNING: /home/vipulkumar/platform/AGL_Needlefish/external/meta-ros/meta-ros-common/recipes-devtools/python/python3-pydot_1.4.1.bb: distutils-common-base.bbclass is deprecated, please use setuptools3-base.bbclass instead
WARNING: /home/vipulkumar/platform/AGL_Needlefish/external/meta-ros/meta-ros-common/recipes-devtools/python/python3-pydot_1.4.1.bb: distutils3.bbclass is deprecated, please use setuptools3.bbclass instead
WARNING: /home/vipulkumar/platform/AGL_Needlefish/external/meta-ros/meta-ros-common/recipes-devtools/python/python3-pydot_1.4.1.bb: distutils-common-base.bbclass is deprecated, please use setuptools3-base.bbclass instead
WARNING: /home/vipulkumar/platform/AGL_Needlefish/external/meta-ros/meta-ros-common/recipes-devtools/python/python3-pydot_1.4.1.bb: distutils3.bbclass is deprecated, please use setuptools3.bbclass instead
WARNING: /home/vipulkumar/platform/AGL_Needlefish/external/meta-ros/meta-ros-common/recipes-devtools/python/python3-pydot_1.4.1.bb: distutils-common-base.bbclass is deprecated, please use setuptools3-base.bbclass instead
WARNING: /home/vipulkumar/platform/AGL_Needlefish/external/meta-ros/meta-ros-common/recipes-devtools/python/python3-pydot_1.4.1.bb: distutils3.bbclass is deprecated, please use setuptools3.bbclass instead
WARNING: /home/vipulkumar/platform/AGL_Needlefish/external/meta-ros/meta-ros1-melodic/recipes-support/opencv/opencv_3.4.5.bb: distutils-common-base.bbclass is deprecated, please use setuptools3-base.bbclass instead
WARNING: /home/vipulkumar/platform/AGL_Needlefish/external/meta-ros/meta-ros-common/recipes-devtools/python/python3-empy_3.3.2.bb: distutils-common-base.bbclass is deprecated, please use setuptools3-base.bbclass instead
WARNING: /home/vipulkumar/platform/AGL_Needlefish/external/meta-ros/meta-ros-common/recipes-devtools/python/python3-empy_3.3.2.bb: distutils3.bbclass is deprecated, please use setuptools3.bbclass instead
WARNING: /home/vipulkumar/platform/AGL_Needlefish/external/meta-ros/meta-ros-common/recipes-devtools/python/python3-empy_3.3.2.bb: distutils-common-base.bbclass is deprecated, please use setuptools3-base.bbclass instead
WARNING: /home/vipulkumar/platform/AGL_Needlefish/external/meta-ros/meta-ros-common/recipes-devtools/python/python3-empy_3.3.2.bb: distutils3.bbclass is deprecated, please use setuptools3.bbclass instead
WARNING: /home/vipulkumar/platform/AGL_Needlefish/external/meta-ros/meta-ros-common/recipes-devtools/python/python3-empy_3.3.2.bb: distutils-common-base.bbclass is deprecated, please use setuptools3-base.bbclass instead
WARNING: /home/vipulkumar/platform/AGL_Needlefish/external/meta-ros/meta-ros-common/recipes-devtools/python/python3-empy_3.3.2.bb: distutils3.bbclass is deprecated, please use setuptools3.bbclass instead
Parsing recipes: 100% |###################################################################################################################################| Time: 0:02:33
Parsing of 5664 .bb files complete (0 cached, 5664 parsed). 7520 targets, 449 skipped, 4 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "2.0.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-agl-linux"
MACHINE = "imx8mq-evk"
DISTRO = "poky-agl"
DISTRO_VERSION = "13.91.0"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
DISTRO_NAME = "Automotive Grade Linux"
ROS_DISTRO = "melodic"
ROS_VERSION = "1"
ROS_PYTHON_VERSION = "2"
meta-pipewire
meta-netboot
meta-app-framework = "HEAD:b5044156fc318a4881e766513871611a560170be"
meta-ros1
meta-ros1-melodic
meta-ros-common
meta-ros-python2 = "master:bfb09373ad8648c3c8d9f34ad13326d354a7d1ab"
meta-python2 = "HEAD:f02882e2aa9279ca7becca8d0cedbffe88b5a253"
meta-qt5 = "HEAD:5b71df60e523423b9df6793de9387f87a149ac42"
meta-agl-demo = "HEAD:08977ac24f2d31b0955786824c9ff62eff981ee9"
meta-freescale = "HEAD:cdd388064845688ac3570aa76a5c01e3df32a67a"
meta-networking
meta-python
meta-filesystems
meta-multimedia
meta-oe = "HEAD:fb7b26b0fb243620f52a61296f4eda6af6ad1af6"
meta-agl-core
meta-agl-core-test
meta-agl-bsp = "HEAD:b5044156fc318a4881e766513871611a560170be"
meta
meta-poky = "HEAD:a5ea426b1da472fc8549459fff3c1b8c6e02f4b5"

Initialising tasks: 100% |################################################################################################################################| Time: 0:00:06
Sstate summary: Wanted 13 Local 0 Mirrors 0 Missed 13 Current 4315 (0% match, 99% complete)
Removing 4 stale sstate objects for arch aarch64: 100% |##################################################################################################| Time: 0:00:00
Removing 1 stale sstate objects for arch imx8mq_evk: 100% |###############################################################################################| Time: 0:00:00
NOTE: Executing Tasks
WARNING: DISTRO_FEATURES:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: DISTRO_FEATURES:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
WARNING: IMAGE_INSTALL:append += is not a recommended operator combination, please replace it.
ERROR: opencv-4.5.5-r0 do_package_qa: QA Issue: non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_calib3d.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_bioinspired.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_videoio.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_photo.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_img_hash.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_shape.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_rapid.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_phase_unwrapping.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_line_descriptor.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_wechat_qrcode.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_alphamat.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_intensity_transform.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_hfs.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_surface_matching.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_tracking.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_imgproc.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_ts.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_face.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_rgbd.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_dnn_objdetect.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_ml.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_structured_light.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_plot.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_stitching.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_imgcodecs.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_saliency.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_sfm.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_dnn.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_fuzzy.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_superres.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_dnn_superres.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_reg.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_core.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_gapi.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_objdetect.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_bgsegm.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_quality.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_flann.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_stereo.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_videostab.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_ccalib.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_mcc.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_ximgproc.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_aruco.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_video.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_barcode.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_highgui.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_features2d.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_dpm.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_datasets.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_optflow.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_xobjdetect.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_xphoto.so'
non -dev/-dbg/nativesdk- package opencv contains symlink .so '/usr/lib/libopencv_xfeatures2d.so' [dev-so]
ERROR: opencv-4.5.5-r0 do_package_qa: Fatal QA errors were found, failing task.
ERROR: Logfile of failure stored in: /home/vipulkumar/platform/AGL_Needlefish/build/tmp/work/aarch64-agl-linux/opencv/4.5.5-r0/temp/log.do_package_qa.19963
ERROR: Task (/home/vipulkumar/platform/AGL_Needlefish/external/meta-openembedded/meta-oe/recipes-support/opencv/opencv_4.5.5.bb:do_package_qa) failed with exit code '1'
NOTE: Tasks Summary: Attempted 9852 tasks of which 9831 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/vipulkumar/platform/AGL_Needlefish/external/meta-openembedded/meta-oe/recipes-support/opencv/opencv_4.5.5.bb:do_package_qa

ラベル(1)
0 件の賞賛
返信
0 返答(返信)