not able to bring up win ce 7 on i.MX51 EVK
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am trying yo bring up WinCE 7 on i.MX51 EVK.
I have compiled the iMX51_EVK_Mobility project and loaded EBOOT into SD card using cfimager.exe application.
EBOOT is coming up and it able to download the image through ethernet interface but it is getting stuck while executing the OS image from RAM.
The Serial output is as follows:
SSI1 = 5644800 Hz
SSI2 = 5644800 Hz
SSI3 = 5644800 Hz
SSI_EXT1 = 10285714 Hz
SSI_EXT2 = 10285714 Hz
USB_PHY = 24000000 Hz
TVE_216_54 = 216000000 Hz
DI = 27000000 Hz
VPU_RCLK = 24000000 Hz
SPDIF0 = 1142857 Hz
SPDIF1 = 1142857 Hz
SLIMBUS = 66500000 Hz
SIM = 66500000 Hz
FIRI = 24000000 Hz
HSI2C = 66500000 Hz
SSI_LP_APM = 22579200 Hz
SPDIF_XTAL = 24000000 Hz
HSC1 = 216000000 Hz
HSC2 = 216000000 Hz
ESC = 15428571 Hz
CSI_MCLK1 = 24629629 Hz
CSI_MCLK2 = 24629629 Hz
ECSPI = 66500000 Hz
LPSR = 0 Hz
PGC = 66500000 Hz
OSC = 24000000 Hz
CKIH_CAMP1 = 22579200 Hz
CKIH2_CAMP2 = 0 Hz
CKIH2 = 0 Hz
FPM = 33554432 Hz
Windows CE Kernel for ARM (Thumb Enabled)
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb
OEMInit: siliconrev = 0x20
BoardID = 0x0.
g_kitlLock = 0x84512BF0
FECInit MAC ADDR 0:4:9F:1:1B:88
FEC is linked, Speed 100Mbps , Full Duplex
KITL will run in interrupt mode
VBridge:: built on [Sep 25 2013] time [15:15:44]
VBridgeInit()...TX = [16384] bytes -- Rx = [16384] bytes
Tx buffer [0x84513FE0] to [0x84517FE0].
Rx buffer [0x84518000] to [0x8451C000].
VBridge:: NK add MAC: [0-4-9F-1-1B-88]
Connecting to Desktop
KITL connected with Desktop
KITL: Leaving polling mode... 0x84513D40
Closing Handle of Timer Thread
&g_kitlLock = 0x84512BF0
VBridge:: VB_INITIALIZED returns [1]
VBridge:: RESET_BUFFER received.
VBridge:: built on [Sep 25 2013] time [15:15:44]
VBridgeInit()...TX = [16384] bytes -- Rx = [16384] bytes
Tx buffer [0x84513FE0] to [0x84517FE0].
Rx buffer [0x84518000] to [0x8451C000].
VBridge:: Current VMini packet filter = [0xB]
can any one help me figuring out the issue.
Thanks
akhil

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I think this is due to Ethernet and kitl connection configuration Please check the WinCE7 Mx51 EVK user guide section Configuring Ethernet Connection for Downloading and Debugging, for steps on how to configure the eboot, also select enable kitl on device boot
Regards