mx6ul ddr clock change?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mx6ul ddr clock change?

ソリューションへジャンプ
1,636件の閲覧回数
mkjasia
Contributor I

We used mx6ul 14x14_evk board and DDR3L.

DDR3L clock operates at 400MHZ by setting mx6ul_14x14_evk_defconfig in u-boot.

We want to change the DDR3L clock to 200MHz.

Please let me know where to modify to change the DDR3L clock.

/*
I am making a custom board and testing it, but the DDR3L clock does not operate at 400 MHz.

Using the DDR stress test provided by NXP, it operates with a clock of 300 MHz.
*/

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,611件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @mkjasia,

I hope you are doing well
 
My apology for the delayed response.
 

Please let me know where to modify to change the DDR3L clock.

=> One can configure the DDR frequency using the RPA file while calibration.
Please look at section 2.1.2 System information from the below document.
 
For more information related to DDR configuration, kindly refer to the below link.
 
Thanks & Regards,
Sanket Parekh

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,612件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @mkjasia,

I hope you are doing well
 
My apology for the delayed response.
 

Please let me know where to modify to change the DDR3L clock.

=> One can configure the DDR frequency using the RPA file while calibration.
Please look at section 2.1.2 System information from the below document.
 
For more information related to DDR configuration, kindly refer to the below link.
 
Thanks & Regards,
Sanket Parekh
0 件の賞賛
返信