mx6ul ddr clock change?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx6ul ddr clock change?

Jump to solution
1,634 Views
mkjasia
Contributor I

We used mx6ul 14x14_evk board and DDR3L.

DDR3L clock operates at 400MHZ by setting mx6ul_14x14_evk_defconfig in u-boot.

We want to change the DDR3L clock to 200MHz.

Please let me know where to modify to change the DDR3L clock.

/*
I am making a custom board and testing it, but the DDR3L clock does not operate at 400 MHz.

Using the DDR stress test provided by NXP, it operates with a clock of 300 MHz.
*/

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
1,609 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @mkjasia,

I hope you are doing well
 
My apology for the delayed response.
 

Please let me know where to modify to change the DDR3L clock.

=> One can configure the DDR frequency using the RPA file while calibration.
Please look at section 2.1.2 System information from the below document.
 
For more information related to DDR configuration, kindly refer to the below link.
 
Thanks & Regards,
Sanket Parekh

View solution in original post

0 Kudos
Reply
1 Reply
1,610 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @mkjasia,

I hope you are doing well
 
My apology for the delayed response.
 

Please let me know where to modify to change the DDR3L clock.

=> One can configure the DDR frequency using the RPA file while calibration.
Please look at section 2.1.2 System information from the below document.
 
For more information related to DDR configuration, kindly refer to the below link.
 
Thanks & Regards,
Sanket Parekh
0 Kudos
Reply