mx6dl android4.3 can support two csi?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mx6dl android4.3 can support two csi?

2,293件の閲覧回数
mrleo
Contributor IV

Hi All:

I know mx6dl support one is csi ,two is mipi_csi.

But I want two csi support one is adv7180,and one is cmos camera.

So I have a problem If the mx6dl support two csi interface or not?

If yes,in android 4.3 system what I should modify ?

Thanks,

Leo

2 返答(返信)

2,120件の閲覧回数
mrleo
Contributor IV

Very Useful!!

Thanks,mx6q can support two csi interface.

imx6dl only have one ipu, one is cis,another is mipi_csi.

2,120件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I think you will find this discussion very helpful.

i.MX6Q : Parallel CSI#2 not working

Best Regards,

Alejandro

0 件の賞賛
返信