multi core debugging

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

multi core debugging

1,395 次查看
saida
Contributor II

I.mx6sabresd board not connecting with core1 and smp but working with core0

DS-5 error message is "unable to connect debugg hardware"

can any one tellme how to debugg two cores ?

Regards

Saida

标签 (1)
0 项奖励
回复
1 回复

1,270 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   by default cores 1-3 are disabled, there is special procedure to

run them. Please look at example codes in

Integrating Processor Expert for i.MX and ARM GCC with Eclipse


Also, You may look at Chapter 3 (Multicore Startup) of "iMX6_Firmware_Guide.pdf"
of the i.MX6 Platfrom SDK. Please create request if You need the SDK, it is not located

on the Web now.

1)    Please open www.nxp.com

2)    On the top level menu, select Support > Sales and Support (http://www.nxp.com/support/sales-and-support:SUPPORTHOME).

3)    On the bottom of the page, select Hardware & Software.

4)    Register with your business email to access the technical NXP online support.

5)    A verification email will be sent to your account. Click the embedded link to verify your access.

6)    On the NXP online support page, select Contact Support from the top menu and click “submit a new case” to start the process.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复