mu irq priority

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mu irq priority

Jump to solution
2,527 Views
panezion
Contributor II

my dev board is imx8mq Evk
is there any document about the mu irq priority.

I’m using rpmsg lite on m4 side and found that the mu irq has almost the highest priority of my running context can I set the mu irq priority like the nvic_xxx way?

Labels (1)
1 Solution
2,491 Views
igorpadykov
NXP Employee
NXP Employee

Hi xiang

one can look at #define APP_MU_IRQ_PRIORITY in

rpmsg-lite/rpmsg_platform.c at master · NXPmicro/rpmsg-lite · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,492 Views
igorpadykov
NXP Employee
NXP Employee

Hi xiang

one can look at #define APP_MU_IRQ_PRIORITY in

rpmsg-lite/rpmsg_platform.c at master · NXPmicro/rpmsg-lite · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,491 Views
panezion
Contributor II

Thank you it's helpful. The priority is define in 

"

#define APP_MU_IRQ_PRIORITY (3U)
21
0 Kudos
Reply