mscale_ddr_stress tool for imx8m mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mscale_ddr_stress tool for imx8m mini

1,234件の閲覧回数
seku
Contributor I

Hi,

1) is there any specific mscale_ddr_stress_tool version for linux_4.9.123? because I've used v2.10, it generates the u-boot lpddr4_timing.c file for u-boot-4.14.78.

2) What are all the DDR files will be generated when I use the mscale_ddr_stress_tool for DDR4 in the ARRAY format? 

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,070件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hi,

Here is the link for the i.MX8M  DDR Stress Tool latest release available,

i.MX8 MSCALE SERIES DDR Tool Release (V2.10) 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信