mmc loading time reduction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mmc loading time reduction

1,747 Views
sachusanal
Contributor III

Dear Sir ,

 

when i am measuring my boot log of kernel i found that 8 seonds time is using for the mmcblk0p1 mount

i am using MFG tool for flashing purpose.

Board:MX6qsabresd board

 

[    8.405572] mmc3: new high speed SDIO card at address 0001

Auto-mount of [/media/mmcblk0p1] successful

[   16.782057] EXT3-fs: barriers not enabled

 

 

could you please help me to reduce the time for create the partition.

i hereby attach the full kernel log here please find out.

Original Attachment has been moved to: printk-log.txt.zip

Labels (1)
0 Kudos
Reply
2 Replies

1,577 Views
jamesbone
NXP TechSupport
NXP TechSupport

As Victor told you in another post that you submit

Actually ext3 filesystem is quite complex and mounting it takes some time.

It may take some significant time even on PC:

root@tecno:~# time mount /dev/sdb1 /mnt/sd

real    0m0.402s

user    0m0.008s

sys     0m0.016s

root@tecno:~#

Here /dev/sdb1 is quite small and fast SD card (4GB class 10 one).

If mounting time is very critical for you you can use other filesystem instead.

However it may cause some compatibility issues.

0 Kudos
Reply

1,577 Views
sachusanal
Contributor III

hi ,

Thanks for your response..

i cant change my  file system.It should .ext3  because we are the finalstage o0f our project

0 Kudos
Reply