mmc loading time reduction

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mmc loading time reduction

1,767件の閲覧回数
sachusanal
Contributor III

Dear Sir ,

 

when i am measuring my boot log of kernel i found that 8 seonds time is using for the mmcblk0p1 mount

i am using MFG tool for flashing purpose.

Board:MX6qsabresd board

 

[    8.405572] mmc3: new high speed SDIO card at address 0001

Auto-mount of [/media/mmcblk0p1] successful

[   16.782057] EXT3-fs: barriers not enabled

 

 

could you please help me to reduce the time for create the partition.

i hereby attach the full kernel log here please find out.

Original Attachment has been moved to: printk-log.txt.zip

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,597件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

As Victor told you in another post that you submit

Actually ext3 filesystem is quite complex and mounting it takes some time.

It may take some significant time even on PC:

root@tecno:~# time mount /dev/sdb1 /mnt/sd

real    0m0.402s

user    0m0.008s

sys     0m0.016s

root@tecno:~#

Here /dev/sdb1 is quite small and fast SD card (4GB class 10 one).

If mounting time is very critical for you you can use other filesystem instead.

However it may cause some compatibility issues.

0 件の賞賛
返信

1,597件の閲覧回数
sachusanal
Contributor III

hi ,

Thanks for your response..

i cant change my  file system.It should .ext3  because we are the finalstage o0f our project

0 件の賞賛
返信