missing some file when I use IAR to develop IMX8 M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

missing some file when I use IAR to develop IMX8 M4

1,332 Views
春华张
Contributor I

hi:

when I use IAR to develop the M4 in IMX8,I can not load project into m4 by j-link.then it will show some file is missing.like that

 

春华张_0-1604456627887.png

春华张_1-1604456650330.png

春华张_2-1604456662620.png

 

 

 

Tags (1)
0 Kudos
Reply
3 Replies

1,325 Views
joanxie
NXP TechSupport
NXP TechSupport

I don't know what imx8 you use, maybe you can try the patch from the link as below:

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=SDK_MX8DXL_3RDPARTY_Patch&appType=file1&...

0 Kudos
Reply

1,318 Views
春华张
Contributor I

thanks for your reply.

I use MIMX8QM ,J-FLASH V6.86f,IAR 7.60.2.

I had get "iar_support_patch_imx8qm".

when I use IAR to debug ,it will say missing some file as these pictures show.

and when I use j-flash to connect the iMX8 ,it will say :

- ERROR: Could not perform target reset
- ERROR: Failed to connect.
Could not perform custom init sequence.

0 Kudos
Reply

1,299 Views
joanxie
NXP TechSupport
NXP TechSupport

my computer doesn't have IAR to test for you, maybe you can refer to the link as below:

"https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F120M-won-t-program-flash-in-IAR/m-p/54..."

0 Kudos
Reply